Question
STM32F103ze Eval Board burning two different programs in two entierly seperate pages
Posted on September 14, 2011 at 14:17
I am using 32F103ze eval board with Ulink 2 Keil JTAG,Is there a method to place two different program into two different location in the internal Flash and burn it using JTAG(one after the other burning process, ie first time first program starting say, 0x08000000, then next other program starting at 0x0800c000, so the second burn should not touch the first programmed area;selective burn)?
thanks, shrinath #two-programs-in-2-exe-region