Skip to main content
leo
Associate
July 15, 2009
Question

STM32F103ZCT6 HardFaultException error ?

  • July 15, 2009
  • 2 replies
  • 776 views
Posted on July 15, 2009 at 08:06

STM32F103ZCT6 HardFaultException error ?

    This topic has been closed for replies.

    2 replies

    joseph239955
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:17

    Could you try change

    _Dly1m = (FuncPtr)0x08010000;

    to

    _Dly1m = (FuncPtr)0x08010001;

    and see if it help?

    leo
    leoAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:17

    Hi all,

    I use STM32F103ZCT6 144pin to add nor flash,

    My main program put in nor flash memory ,and procedure that often uses put in STM32F103ZCT6 flash memory(ex, LCD function delay function).

    when main program call delay function,

    if I use debug ''Step Into'' is ok,

    but I use debug ''Go'', Error appears, into ''HardFaultException()''.

    STM32F103ZCT6 flash memory code:

    use stm32f10x_flash.icf

    add

    ''define symbol __ICFEDIT_region_Dly1m_start__ = 0x08010000;''

    ''define symbol __ICFEDIT_region_Dly1m_end__ = 0x08010040;''

    ''place at address mem:__ICFEDIT_region_Dly1m_start__ { readonly section Dly1m };''

    my delay.h

    #pragma location=''Dly1m''

    void _Dly1m(void);

    //========================================================

    Nor flash memory code:

    use stm32f10x_nor.icf

    my main.c

    typedef void (*FuncPtr)(void);

    FuncPtr _Dly1m;

    viod main(void)

    {

    _Dly1m = (FuncPtr)0x08010000;

    :

    :

    _Dly1m(); // ''Step Into'' is ok,but ''Go'' is Error.

    :

    :

    }

    [ This message was edited by: leo.chang on 14-07-2009 13:46 ]