Skip to main content
amore
Associate
August 7, 2013
Question

STM32F103VET6 ,converts RGB/YCrCb image data to JPEG

Posted on August 07, 2013 at 10:12

Can you help me a little bit?My thesis is about writing the code for image compression and decompression on STM32F103VET6. I have a RGB file and my tasks are writing 1 code to convert the RGB to a JPEG and writing 1 more code to compress the above JPEG into a smaller packet for transmission through the 3G network using SIM5218.The receive side uses the STM32 hardware which can extract file into JPEG format.So, is it available if I only use the STM32? or any ic DSP else? Could you share the code for me if you have, please?My mail is: duongtuananh.hust @gmail.com. Thank you so much!

#stm32 #rgb #jped #decode #ov767
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    August 7, 2013
    Posted on August 07, 2013 at 16:51

    I'm a little confused about whose thesis/project this really is?

    Take the STM32 out of the equation, can you do any of the tasks in C, on your desktop?
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    amore
    amoreAuthor
    Associate
    August 8, 2013
    Posted on August 08, 2013 at 19:21

    amore
    amoreAuthor
    Associate
    August 8, 2013
    Posted on August 08, 2013 at 20:09

    This is my thesis: Using MCU STM32VET6 communicates with OV7670 Camera, the returned format is RGB565 sized 320x240 pixel. 1 image formats RGB565 about 150kb for one 0.3Megapixel image. Now I want to turn images into JPEG format and compress them about 15KB/1 image so I can transmit them in 3G network using sim5218. the algorithms of the image compression are implemented rightly on the hardware, it means that MCU STM32 directly does the algorithms of the image compression from RGB565 into JPEG or uses more IC specialized in compressing images.my problems are I do not have the algorithms of compression on STM32 and do not also know which IC should be used for the above project. Really hope that you guys will help me! Thank you so much

    Tesla DeLorean
    Guru
    August 8, 2013
    Posted on August 08, 2013 at 20:45

    I got that part, but if it's your thesis, then this is basic work you should be doing, and studying.

    The STM32 does not provide any hardware support for image compression/decompression. Some cameras can output JPEG or M-JPEG type data.

    Is this a master's thesis? Are you expected to code the JPEG algorithm from scratch, use the reference algorithm, or use some third-party library with an API to manipulate image data?

    If you need a JPEG implementation in C, aren't there examples out there that do this? Can you not recompile those for the STM32, MIPS, whatever platform? Do you have to write this is assembler? Does it have to be fast/efficient? Where is 150 KB of data going to get held?

    Are there not companies selling image processing software that support JPEG, that you could utilize?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..