Skip to main content
doss
Associate
March 17, 2019
Question

STM32F103VCT6 more RAM+Flash than datasheet says?

  • March 17, 2019
  • 4 replies
  • 1729 views

Hi,

today I stumbled across a problem, where I wanted to assign around 50k of RAM to FreeRTOS and I immediately got a linker error, because target ran out of RAM.

I had a look at the datasheet and this says 48k RAM. I've been using a self-hacked-together linkerscript for very long now, that has 64k set.

For a long time now I was thinking it has 64k, because my flash programming utilities report it every time I program this chip.

I am using a ST-LinkV2, host-OS is linux and I use texane's stlink utility. I also tried with stm32flash and stm32loader.py.

This is what they report:

st-info from texane's st-link utility reports 64k RAM, 256k flash

$ st-info --probe
Found 1 stlink programmers
 serial: 513f6f06503f55493945093f
openocd: "\x51\x3f\x6f\x06\x50\x3f\x55\x49\x39\x45\x09\x3f"
 flash: 262144 (pagesize: 2048)
 sram: 65536
 chipid: 0x0414
 descr: F1 High-density device

stm32flash reports 64k RAM and 512k FLASH:

$ stm32flash /dev/ttyUSB0 
stm32flash 0.5
 
http://stm32flash.sourceforge.net/
 
Interface serial_posix: 57600 8E1
Version : 0x22
Option 1 : 0x00
Option 2 : 0x00
Device ID : 0x0414 (STM32F10xxx High-density)
- RAM : 64KiB (512b reserved by bootloader)
- Flash : 512KiB (size first sector: 2x2048)
- Option RAM : 16b
- System RAM : 2KiB

stm32loader.py does not report sizes:

$ sudo ./stm32loader.py -V -p /dev/ttyUSB0 
Open port /dev/ttyUSB0, baud 115200
*** Get command
 Bootloader version: 0x22
 Available commands: 0x0, 0x1, 0x2, 0x11, 0x21, 0x31, 0x43, 0x63, 0x73, 0x82, 0x92
Bootloader version 22
*** GetID command
Chip id: 0x414 (STM32 High-density)

Is this a false report? I assume the serial bootloader (in case of stm32flash) reports the memory sizes to the tool. Also I assume ST wouldn't program wrong memory sizes to the bootloader. Does this mean my device has 64k/512k?

Does the internal bootloader scan flash for availability or does it work with pre-programmed flash/ram-size values?

How does the ST-LinkV2 (swdio/swdclk connection) work? It detects 256k flash (as this device is supposed to have), but it detects 64k RAM (16k more than supposed).

How would I test for this? Writing an application, that writes and reads back RAM above 48k and same for the flash?

I already heard about the 128k STM32F103C8T6 (blue pills etc) that have 128k flash. Maybe it is the same with these..,

Thanks in advance,

Doss

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
March 17, 2019

Depends on the die, ST has a handful of die covering all F1 series parts. Smaller memory ones typically targeting smaller packages, as the RAM/FLASH are physically quite large in area.

ST test a portion on some parts, depending on pricing structure, and encode that size in the OTP. For 0x414 die this would be the 16-bit word at 0x1FFFF7E0

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
doss
dossAuthor
Associate
March 18, 2019

0x1FFFF7E0 says 0x0100. I haven't found a description of this word yet. Could you please point me to the document where I can find more about this memory location?

I've been playing around with openocd and set flashsize to 0 (probe instead of predefined) and tried to write a 512k file with just 0xA5A5.... in it. It stops with a error (something like "bank not supported" or similar) when it reaches 256k+1b.

The same if I tell openocd it has 512k instead of probing.

With RAM I had success.

I wrote a test-program that writes+reads this 16k chunk of memory.

Official RAM is at 0x20000000-0x2000BFFF (48k). The rest up to 0x2000FFFF is (almost) working RAM.

The test program freezes whenever I try to read or write above 0x2000FFFC. Up to and including 0x2000FFFC I have usable RAM.

This is my test code:

int main(void) {
 char buffer[81];
 uint32_t address, misses = 0;
 volatile uint32_t *dptr; 
 
 rcc_clock_setup_in_hse_8mhz_out_72mhz();
 
 init_usart1(); 
 usart1_puts("\e[2J\e[0;0H"); // clear screen + home cursor on terminal
 usart1_puts(" testing address 0x");
 usart1_puts("\e[s"); // tell terminal to save cursor position
 
 for(address = 0x2000C000; address <= 0x2000FFFC; address++) {
 snprintf(buffer, 81, "%08lX", address);
 usart1_puts(buffer);
 usart1_puts("\e[u"); // go to saved cursor position for next address to print
 
 dptr = (volatile uint32_t *)address;
 *dptr = 0xA5A5A5A5;
 if(*dptr != 0xA5A5A5A5)
 misses++;
 }
 
 snprintf(buffer, 81, "\r\n\r\n [ misses = %lu ] \r\n", misses);
 usart1_puts(buffer);
 
 while(1) { }
 
 return 0;
}

Tesla DeLorean
Guru
March 18, 2019
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
doss
dossAuthor
Associate
March 18, 2019

Thank you!