stm32f103ret6 flash erase problem
Hi,
I need to perform STM32F103RET6 flash memory operation: erase, write. My erase failed. Anybody has the EWARM project for internal bootloader(burnt to chip from factory)? Or any working flash routines for STM32F103RET6?
I am using \AN4657-STM32Cube_IAP_using_UART\Projects\STM3210C_EVAL\IAP_Main project. And change USER_FLASH_END_ADDRESS from 0x08040000 to 0x08080000 to match the flash for STM32F103RET6. I think this is the only change for the STM32F103RET6 device from STM32F107 device. All other #define macro should be the same.
But when I execute the statement “FLASH_If_Erase(APPLICATION_ADDRESS);� the program still went to Hard_Fault function.
My code is:
int main(void) {
HAL_Init();
SystemClock_Config();
FLASH_If_Init();
FlashProtection = FLASH_If_GetWriteProtectionStatus(); // return to 0 indicate not write protected.
FLASH_If_Erase(APPLICATION_ADDRESS);
while(1) {}
}
void SystemClock_Config(void)
{
RCC_ClkInitTypeDef clkinitstruct = {0};
RCC_OscInitTypeDef oscinitstruct = {0};
oscinitstruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
oscinitstruct.HSEState = RCC_HSE_ON;
oscinitstruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
oscinitstruct.PLL.PLLState = RCC_PLL_ON;
oscinitstruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
oscinitstruct.PLL.PLLMUL = RCC_PLL_MUL6; // 8MHz*6=48MHz
if (HAL_RCC_OscConfig(&oscinitstruct)!= HAL_OK)
{
sys_err_code |= ERR_RCC_OSC_CONFIG;
}
clkinitstruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
clkinitstruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
clkinitstruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
clkinitstruct.APB2CLKDivider = RCC_HCLK_DIV1;
clkinitstruct.APB1CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&clkinitstruct, FLASH_LATENCY_2)!= HAL_OK)
{
sys_err_code |= ERR_RCC_CLK_CONFIG;
}
RCC->CFGR &= ~0x0000C000;
RCC->CFGR |= 0x00008000; // pclk2/6 as ADC clock(=48/6=8MHz)
}