Associate III
March 19, 2013
Question
STM32F103RB I2C problem
- March 19, 2013
- 5 replies
- 1250 views
Posted on March 19, 2013 at 13:12
And here the screen shot of 0x40:
And here the screen shot of 0x41: (nothing changes)
I also tried another number like 0x48 and 0x49 and its the same too. I dont know what to do.
Bye bye
Hi,
I am trying to comunicate with MCP23016 by i2c and i am using STM32F103RB with uVision 4. The problem is that if I send 0x40 is the same if I send 0x41. Its the red mark on the code. My code is:void I2C_Configuration(void)
{
I2C_InitTypeDef I2C_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);
/* Configure I2C1 pins: SCL and SDA */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Enable I2C1 reset state */
RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C1, ENABLE);
/* Release I2C1 from reset state */
RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C1, DISABLE);
/* I2C configuration */
I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;
I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;
I2C_InitStructure.I2C_OwnAddress1 = I2C1_SLAVE_ADDRESS7;
I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;
I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
I2C_InitStructure.I2C_ClockSpeed = 100000;
/* Apply I2C configuration after enabling it */
I2C_Cmd(I2C1,ENABLE);
I2C_Init(I2C1, &I2C_InitStructure);
}
unsigned int read_MCP(u8 WriteAddress, u8 cmdByte, u8 ReadAddress, u8 NumByteToRead) {
int lsbdata, msbdata;
unsigned int ldata;
int timeout=0;
int indice;
while(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY));
I2C_GenerateSTART(I2C1, ENABLE); /* Send I2C1 START condition */
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); /* Test on I2C1 EV5 and clear it */
I2C_Send7bitAddress(I2C1, 0x40, I2C_Direction_Transmitter);
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); /* Test on EV6 and clear it */
I2C_ClearITPendingBit(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED);
I2C_SendData(I2C1, GP0); //CONFIGURA PARA LEITURA
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));
I2C_GenerateSTOP(I2C1, ENABLE);
DelayUs(100);
I2C_GenerateSTART(I2C1, ENABLE); /* Send I2C1 START condition */
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); /* Test on I2C1 EV5 and clear it */
I2C_Send7bitAddress(I2C1,0x41
, I2C_Direction_Transmitter);
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); /* Test on EV6 and clear it */
I2C_ClearITPendingBit(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED);
while(!I2C_GetFlagStatus(I2C2, I2C_FLAG_RXNE));
lsbdata = I2C_ReceiveData(I2C2);
I2C_ClearITPendingBit(I2C1, I2C_FLAG_RXNE);
while(!I2C_GetFlagStatus(I2C2, I2C_FLAG_RXNE));
msbdata = I2C_ReceiveData(I2C2);
I2C_ClearITPendingBit(I2C1, I2C_FLAG_RXNE);
I2C_GenerateSTOP(I2C1, ENABLE);
ldata = (msbdata<<8);
ldata = ldata + lsbdata;
return(ldata);
}
Thats what mcp23016 needs.
And here the screen shot of 0x40:
And here the screen shot of 0x41: (nothing changes)
I also tried another number like 0x48 and 0x49 and its the same too. I dont know what to do.
Bye bye