Skip to main content
felipe
Associate III
April 11, 2013
Question

STM32F103RB CAN PINS PROBLEM

  • April 11, 2013
  • 4 replies
  • 798 views
Posted on April 11, 2013 at 16:03

Hi,

I have a problem with the CAN keil example for mcbstm32 board.

I use this example a lot with the remap for CAN so the pins are PB8 and PB9. That is theDefault configuration for the board.

I tried to change the pins to original position with no remap (PA11 and PA12) to test the program with another board.

So I go to CAN_STM32Fc and change the function to:

/* 1. Enable CAN controller Clock */

RCC->APB1ENR |= (1 <<

25

);

/* Note: MCBSTM32 uses PB8 and PB9 for CAN */

/* 2. Setup CAN Tx and Rx pins */

// RCC->APB2ENR |= (1 <<

0

); // enable clock for Alternate Function

// AFIO->MAPR &= 0xFFFF9FFF; // reset CAN remap

// AFIO->MAPR |= 0x00004000; // set CAN remap, use PB8, PB9

/* GPIOB clock enable */

// RCC->APB2ENR |= (1 <<

3

);

/* Configure CAN pin: RX PB.8 input push pull */

// GPIOB->CRH &= ~(0x0F<<

0

);

// GPIOB->CRH |= (0x08<<

0

);

/* Configure CAN pin: TX PB.9 alternate output push pull */

// GPIOB->CRH &= ~(0x0F<<

4

);

// GPIOB->CRH |= (0x0B<<

4

);

/* 2. Setup CAN Tx and Rx pins */

/* GPIOA clock enable */

RCC->APB2ENR |= (1 <<

2

);

/* Configure CAN pin: RX PA.11 input push pull */

GPIOA->CRH &= ~(0x0F<<

12

);

GPIOA->CRH |= (0x08<<

12

);

/* Configure CAN pin: TX PA.12 alternate output push pull */

GPIOA->CRH &= ~(0x0F<<

16

);

GPIOA->CRH |= (0x0B<<

16

);

/* 3. Setup IRQ vector for CAN interrupt */

/* not necessary */

/* 4. Enable CAN interrupt */

NVIC->IPR [4] |= 0x10000000; /* set priority lower than SVC */

NVIC->ISER[0] |= (1 << (USB_HP_CAN_TX_IRQChannel & 0x1F));

/* only FIFO 0 is used */

NVIC->IPR [5] |= 0x00000010; /* set priority lower than SVC */

NVIC->ISER[0] |= (1 << (USB_LP_CAN_RX0_IRQChannel & 0x1F));

return CAN_OK;

It compile ok but after callingCAN_Start it stucks.

The example is: C:\Keil\ARM\Boards\Keil\MCBSTM32\RL\CAN

Any ideas?

Thanks

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    April 11, 2013
    Posted on April 11, 2013 at 19:38

    There is definitely an errata relating to USART1 CTS/RTS usage on PA11/12 and CAN1 interfering, but not sure it impacts CAN1. There is USB here too.

    Does the port work in loop-back mode? Do you have transceivers requiring separate enablement?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    felipe
    felipeAuthor
    Associate III
    April 11, 2013
    Posted on April 11, 2013 at 19:54

    The loop back doesnt work and the tranceiver is SN65HVD230DR.

    Where can  I found this errata?

    Tesla DeLorean
    Guru
    April 11, 2013
    Posted on April 11, 2013 at 20:03

    Where can  I found this errata?

    Google STM32 Errata? It's on the website with the other product docs.

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/errata_sheet/CD00190234.pdf

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    felipe
    felipeAuthor
    Associate III
    April 11, 2013
    Posted on April 11, 2013 at 20:35

    Sorry I thought that was other errata.

    Seems that its not my problem.

     

    In some specific cases, some potential weakness may exist between alternate functions mapped onto the same pin.

     

    2.6.1 USART1_RTS and CAN_TX

     

    Conditions

     

    �? USART1 is clocked

     

    �? CAN is not clocked

     

    �? I/O port pin PA12 is configured as an alternate function output.STM32F10xxx silicon limitations Errata sheet

     

    14/36 Doc ID 14574 Rev 11

     

    Description

     

    Even if CAN_TX is not used, this signal is set by default to 1 if I/O port pin PA12 is 

     

    configured as an alternate function output.

     

    In this case USART1_RTS cannot be used.

     

    I will probably just use the pins PB8 and PB9 for CAN.

    Thanks