Skip to main content
Associate II
Oct 30, 2024 10:15 AM UTC
Solved

STM32F103C8T6 Bluepill giving Windows "Device Descriptor Request Failed"

Hi all,

Total newbie here.

I am seeing this error in Windows 11 Device Manager: "Device Descriptor Request Failed", when I plug the Bluepill to a PC using Bluepill's onboard micro-USB Port

Windows Error.jpg

Although the Bluepill looks like it is running OK with the previously flashed program (Blink PC13) with power supplied via the Bluepill's onboard micro-USB, Windows is giving this error.

 

Being a "perferctionist", I would like to see the Windows error eliminated.

I have check few "solutions" on youtube and none of them seems to apply to STM32, and thus not working.

 

Can any kindly soul please help.

 

Sorry if this has been asked before, but being a newbie to this site, I can't find anything suitable.

This topic has been closed for replies.
Thomas8Best answer
Visitor II
Oct 30, 2024 4:48 PM UTC

How do you know his blue pill has a fake chip soldered? There are lot of BP boards with chips from other manufacturer. Moreover this error also happens with a original chip. Thats because ST simply forgot to integrate a switchable 1k5 connect resistor. So the BP adds a 1K5 resistor from PA12 to V3.3.

The downside of this is the host sees a new connected USB device and tries to enumerate it. This of course fails when no usb firmware is loaded. 

There are 2 possible solutions:

1. use a usb cable with VBUS and GND only so there are no D+ and D- connection. (Charge only cable) to power the BluePill board.

2. set PA12 to output and PA12 to low so the host cant see the 1k5 resistor

 // Pin PA12 as Open Drain Output 
 GPIOA->CRH &= ~(0b1111 << 16);
 GPIOA->CRH |= (0b0110 << 16);
// set PA12 low
GPIOA->ODR &= ~(1 << 12);

 dont forget to set PA12 back to floading input before you want to use USB.

 GPIOA->CRH &= ~(0b1111 << 16);

thats all

20 replies

Peter BENSCH
ST Technical Moderator
Oct 30, 2024 12:08 PM UTC

Welcome @JLHK01, to the community!

If you use the search function of the community and search for ‘blue pill’, you will find a lot of similar questions. You will also very often find answers such as: ‘blue pill is not a product of STMicroelectronics and has only been using counterfeit STM32F103 for years’. This means that you should ask the manufacturer of the blue pill or the counterfeit, not the manufacturer of the original STM32F103.

You can also convert the Blue Pill: simply unsolder the counterfeit and fit an original STM32F103C8T6 - you are immediately compatible and you will be gladly helped here.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Oct 30, 2024 12:35 PM UTC

@JLHK01 You could also get a Nucleo board, and be sure that you have a genuine & supported board & chip - plus you get a free genuine ST-Link thrown in!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JLHK01Author
Associate II
Oct 31, 2024 5:46 AM UTC

Andrew,

The only NUCLEO candidate I can find is the NUCLEO-F103RB.

But I don't need a 64 pin MCU and I don't need 128K Flash.

Afterall, the board is too big / expensive for my final "deployment" after project,

JLHK01Author
Associate II
Oct 30, 2024 1:56 PM UTC

Thanks Peter and Andrew for your reply.

As a total newbie, I didn't know that bluepill is not a ST product. I thought it is a nickname of a developemnt board by ST.

My apologies and sorry for the disturbace.

Anyway, thanks for your advices.

Peter BENSCH
ST Technical Moderator
Apr 25, 2025 6:41 AM UTC

ST resources are only dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes products work properly with the firmware we provide.

We recommend to purchase genuine products from STMicroelectronics and purchase them from known and trusted distributors.

This thread will now be locked. However, if you face difficulties while using genuine ST products, we’re here to assist you. Please feel free to start a new thread, and our team, along with community members, will be ready to help you with any issues/questions you encounter.

Thank you for your understanding.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.