Skip to main content
tom239955_stm1_st
Associate
May 12, 2008
Question

STM32F103C6T6-Flash Loader Demonstrator

  • May 12, 2008
  • 24 replies
  • 3461 views
Posted on May 12, 2008 at 07:25

STM32F103C6T6-Flash Loader Demonstrator

    This topic has been closed for replies.

    24 replies

    niksa
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    We are experiencing the exactly same problem, on the same chip. Just tried Flash Loader version 1.1, and it does not help. With Flash Loader 1.1, we can see the following:

    - if we select Erase option, and manually select the pages to erase, the erase procedure will finish

    - after that, when we open the window to manually select which pages to erase, we can see that all pages have READ protection enabled (red lock icon is displayed)

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    Hi

    Could you use the command line software instead posted here :

    http://www.st.com/mcu/forums-cat-6720-23.html&start=10

    and let me know if you have the same issue.

    Cheers,

    STOne-32.

    tom239955_stm1_st
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    STOne-32,

    I've been using the STM32 Command Line Loader, and it seems all is OK.

    My board has been having no problems with all the normal functions, erase/prog/verify ect!

    Thankyou very much for your help, hope to see a new GUI soon!

    Kind Regards

    Tom

    niksa
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    My colleague has posted more detailed problem description to a separate thread, we will try the command line tool and reply there.

    http://www.st.com/mcu/forums-cat-6811-23.html

    Thanks,

    Niksa