Skip to main content
vinay
Associate
February 11, 2015
Question

STM32F103C6 SPI to dataflash(M25p80) sending & receiving problem

  • February 11, 2015
  • 3 replies
  • 1150 views
Posted on February 11, 2015 at 14:51

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    3 replies

    stm322399
    Senior
    February 11, 2015
    Posted on February 11, 2015 at 15:10

    Did you enable SPI1 peripheral clock ?

    Can you observe SCK on PA5 with an o-scope ?

    vinay
    vinayAuthor
    Associate
    February 12, 2015
    Posted on February 12, 2015 at 12:10

    Yes ,

     clock was enabled and PA5 clock signal also getting on o-scope,But instead of 72 MHZ am getting only 64MHZ of clock frequency. I think that is not issue for SPI, Because SPI can able to run with maximum 50MHZ not more than that.

    Problem is data not getting into SPI_DR register .Remaining all SPI registers are working properly.

    If you have any clarity about the issue please help me out Sir.

    stm322399
    Senior
    February 12, 2015
    Posted on February 12, 2015 at 14:00

    First advice: avoid running at 72 or 64 MHz during troubleshooting session, stay at 10MHz max

    Second advice: show use code with all macro define necessary to understand. Example: what is SPI1 ? Is this SPI1 as defined in ST  CMSIS device header file (a pointer to a structure defining SPI registers) ? Or is SPI1 an integer that you use to index the p_stfSPIReg_all device table ? This is not clear, and maybe the source of your bug.

    Show us all function that you use that are not from SPL or HAL:

    SPI_Init (same name as SPL but not same argument type), and others.

    Last, tell us where you are blocked:

    /* Wait to receive a byte */

      while (SPI_GetFlagBitStatus(SPI1, SPI_RXEN_INTERRUPT) == SPI_FLAGBIT_RESET);

    or

    // wait until transmit complete

    while(!(p_stfSPIReg_all[en_lDev]->SPI_SR & SPI_SR_RXNE_MASK ));