Skip to main content
Jason Smith
Associate II
Apr 2, 2017 2:42 PM UTC
Question

STM32F103 - Std Periph Driver not working with bootloader

Posted on April 02, 2017 at 16:42

I am fairly new to ARM and I am running into an issue with the ST Standard Peripheral Driver. If I download my project to my STM32F103 at Vector 0x08000000, it runs fine. If I use my bootloader to load my project to 0x08004000 (I set this in the linker tab as well using Keil), it will not work. Other projects work fine when using the bootloader at 0x08004000 but this project is my first one with the Std. Periph. Driver. Does the driver expect vector 0x08000000 somewhere that I need to edit a source or header file?  Or is some other issue going on here?

    This topic has been closed for replies.

    1 reply

    antonius
    Associate III
    Apr 3, 2017 9:35 AM UTC
    Posted on April 03, 2017 at 11:35

    You better use STM32CubeMx and test with playing on GPIO for the first time and HSI (internal clock)