Skip to main content
wb0gaz
Associate III
June 30, 2022
Question

STM32F103 (stand-alone, not on "blue pill" board) - ADC uncertainty when reading internal reference (channel 17)?

  • June 30, 2022
  • 2 replies
  • 1209 views

Problem type - ADC readings excess uncertainty when reading internal reference (channel 17) - got to this point after excess ADC reading uncertainty on device pins, trying to isolate cause.

Hardware Details - small 2-layer board (about the size of a LQFP48/DIP adapter module), VSS and VSSA (4 places) to ground within a few mm, VDD and VDDA (4 places) each with 0.1 uF 0805 decoupling cap within a few mm, then on to 3.3V power source. Reset is pulled up (47K) to 3.3V power source. PA14/PA15 tied to STLINK device (STLINK device is not providing power to the target.) BOOT0 tied to 3.3V source. All other pins open.

Software details - bare-metal configuration of CPU - 24 MHz CPU clock (RC, not crystal)

   // Initialize

   if ((ADC1->CR2 & ADC_CR2_ADON) == 0) // ADC not turned on, so initialize

   {

      RCC->APB2ENR |= RCC_APB2ENR_ADC1EN; // Turn on ADC1 clock

      ADC1->CR2 = 0x00800001; // Turn on Vref, Temp and ADC itself

      for (uint16_t volatile i = 0; i < 10000; i++); // Delay after turn-on

      ADC1->CR2 = 0x00800005; // Turn on CAL, keep Vref, Temp and ADC itself on

      while ((ADC1->CR2 & ADC_CR2_CAL) != 0); // Wait cal complete

      ADC1->SMPR1 = (7 << ADC_SMPR1_SMP17_Pos) | (7 << ADC_SMPR1_SMP16_Pos); // ADC 16, 17 set to 239.5 cycle sample time)

      ADC1->SMPR2 = 0x3FFFFFFF; // ADC 0..9 set to 239.5 cycle sample time

   }

   // Single read from channel 17 (reference voltage)

   ADC1->SQR3 = 17; // Read reference voltage

   ADC1->CR2 |= ADC_CR2_ADON; // Start conversion

   while ((ADC1->SR & ADC_SR_EOC) == 0); // Wait end of conversion

   uint16_t adcsample = ADC1->DR;

Observation - readings are scattered over about +/- 10 counts.

Is this indicating that VDDA (which is currently tied to VDD_1, VDD_2 and VDD_3) is encountering noise?

Happy to provide any clarifications or improvements to problem statement.

Thank you.

This topic has been closed for replies.

2 replies

wb0gaz
wb0gazAuthor
Associate III
June 30, 2022

Considerable progress - added 27 uH 0805 inductor in series between VDD_1/2/3 and VDDA, modest improvement in distribution of the samples was seen. Then changed the decoupling cap between VDDA and ground from 0.1 uF to 10 uF (ceramic 0805 6.3V) and saw a dramatic improvement. Finally changed 0.1 uF decoupling cap near VDD_1 from 0.1 uF to 10 uF, and saw a further modest improvement in distribution of samples. Lesson learned - can't take the value of decoupling caps in this area for granted!

Reading Vref 65k times with 239.5 sample time and 12 MHz ADC clock

First plot is after changes (MCU now has 10 uF @ VDD_12 to ground; VDDA supplied by same 3.3V source, but with 27 uH series inductance followed by 10 uF @ VDDA to ground).

Second plot is before changes (VDDA tied to VDD_1, 0.1 uF at both pins to ground)

0693W00000QKDRiQAP.png0693W00000QKDRYQA5.png

Michal Dudka
Lead
July 1, 2022

ST appnotes suggest 1uF//10nF parallel combination to VDDA-VSSA. Series inductance can help. But ADC "noise" highly depends on external conditions, like quality yours 3.3V supply, grounding scheme etc.

Yours results with 27uH, looks nice. I don't believe it can get any better.