Skip to main content
nmamore
Associate II
July 14, 2021
Question

STM32F103 Reduce VBAT Current

  • July 14, 2021
  • 4 replies
  • 1498 views

My datasheet (STM32F103VC) states the Vbat current draw is 1.4uA. Is there a way to reduce this? I only need the backup domain for RTC/LSE. I know there are many backup registers as well. Could I turn these off to reduce current draw?

This topic has been closed for replies.

4 replies

TDK
July 14, 2021

The backup domain cannot be partially disabled.

"If you feel a post has answered your question, please click ""Accept as Solution""."
nmamore
nmamoreAuthor
Associate II
July 14, 2021

Thank you. Are you familiar with any possible ways that I could further reduce current draw?

TDK
July 14, 2021

You could reduce the voltage to the minimum allowed. I don't think there's anything else you can do apart from that, but I'm not an expert in low power applications.

Logically, if there were something easy that could be done to reduce the current, it would be silly of them not to use the lower value in the datasheet.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
July 14, 2021

Use a different STM32 model, e.g. 'L4 - you can have mostly pin and function compatibility and roughly 2-3x lower IVBAT.

Most of the current goes to LSE/RTC. For even lower battery consumption use a well-chosen external RTC.

JW