Skip to main content
WTetl.2
Associate II
January 26, 2024
Solved

STM32F103: Intended behaviour of HAL_ADC_Start_DMA

I have a program where I am trying to scan over 8 ADC channels on ADC1, take 10 samples from each and transfer to the DMA. From everything I have read, I cannot enable DMA Continuous Conversion on STM32F103, so I will need to use discontinuous scan mode.

It appears that when I run HAL_ADC_Start_DMA, it only does a single conversion, rather than the 80 I would expect (I have buffer size set to 80). The only way I can get HAL_ADC_ConvCpltCallback to be called (which should indicate 10 scans) is to execute HAL_ADC_Start_DMA 80 times. Furthermore, all 80 measurements in the buffer are of the first channel in the rank order, meaning it's not remembering where it was in the sequence.

I can't imagine that this is the intended behavior of the ADC. Something must be stopping the ADC after it does only one conversion and it doesn't even get to move onto the second one in the sequence.

The relevant part of my main.c (which fills the buffer every 80 ms) is below, I have taken out parts that do not have to do with ADC/DMA to shorten the excerpt:

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2022 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.

 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define BUFFER_SIZE 80 // 8 channels * 10 measurements per round
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

/* USER CODE BEGIN PV */
/*Variables and arrays for operation */
uint16_t adcBuffer[BUFFER_SIZE];
uint16_t counter = 0;
uint32_t tick = 0;

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_DMA_Init(void);
static void MX_ADC1_Init(void);

/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 /* USER CODE BEGIN 2 */
 
 HAL_ADCEx_Calibration_Start(&hadc1)
	
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */

	 HAL_Delay(1);

	 tick = tick + 1;

	 if (HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adcBuffer, BUFFER_SIZE) != HAL_OK)
	 	{
	 		/* Start Error */
		 Error_Handler();
	 	}
 }
 /* USER CODE END 3 */

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = ENABLE;
 hadc1.Init.NbrOfDiscConversion = 1;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 8;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_8;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_9;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_10;
 sConfig.Rank = ADC_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_11;
 sConfig.Rank = ADC_REGULAR_RANK_4;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_12;
 sConfig.Rank = ADC_REGULAR_RANK_5;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_13;
 sConfig.Rank = ADC_REGULAR_RANK_6;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_14;
 sConfig.Rank = ADC_REGULAR_RANK_7;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_15;
 sConfig.Rank = ADC_REGULAR_RANK_8;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

 hdma_adc1.Instance = DMA1_Channel1;
 hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
 hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
 hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
 hdma_adc1.Init.Mode = DMA_CIRCULAR;
 hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH;

 if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
 {
	 Error_Handler();
 }
 __HAL_LINKDMA(&hadc1, DMA_Handle, hdma_adc1);
}

/* USER CODE BEGIN 4 */

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc1)
{
 // This function is automatically called when DMA completes a transfer
	counter = counter + 1;
	HAL_GPIO_TogglePin(STATUS_GPIO_Port, STATUS_Pin);
}

/* USER CODE END 4 */

 

Any help would be appreciated.

This topic has been closed for replies.
WTetl.2
WTetl.2Best answer
Associate II
January 29, 2024

This got me thinking though, I just disabled discontinuous conversion mode altogether and it is working as intended. There is no need to enable discontinuous if you want all of the conversions done at once anyway.

 

 hadc1.Instance = ADC1;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 8;

 

3 replies

raptorhal2
Lead
January 27, 2024

Set the Number Of Discrete conversions to 0.

Set the ADCBuffersize to 8.

Set up an 8x10 buffer.

Start the ADC/DMA, wait for the end of conversion, then save the 8 values in the 8x10 buffer.

Repeat the start 10 times.

WTetl.2
WTetl.2Author
Associate II
January 29, 2024

Thank you for your replay raptorhal. The configurator says that Number of Discontinuous Conversions must be between 1 and 8. I set it to 0 in main.c anyway and now it does not do any conversions at all. The HAL library says that the parameter is

"Specifies the number of discontinuous conversions in which the main sequence of regular group (parameter
NbrOfConversion) will be subdivided. If parameter 'DiscontinuousConvMode' is disabled, this parameter is
discarded. This parameter must be a number between Min_Data = 1 and Max_Data = 8."

Wouldn't setting it to 0 cause a division by 0? Did you mean a different parameter?

WTetl.2
WTetl.2AuthorBest answer
Associate II
January 29, 2024

This got me thinking though, I just disabled discontinuous conversion mode altogether and it is working as intended. There is no need to enable discontinuous if you want all of the conversions done at once anyway.

 

 hadc1.Instance = ADC1;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 8;