Skip to main content
L C
Associate III
April 23, 2017
Question

STM32F103 ILI9341 non-arduino example request

Posted on April 23, 2017 at 02:47

Hello!

I want to control ILI9341(SPI LCD) by STM32F103C8.

Simple SPI access is ok.

Most example are belong arduino in internet, but I am using EWARM.

Please share your experience to me.

BR

LC

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    April 23, 2017
    Posted on April 23, 2017 at 03:17

    Googling STM32 ILI9341 dumped a bunch of hits

    https://github.com/fagcinsk/stm-ILI9341-spi

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    L C
    L CAuthor
    Associate III
    April 25, 2017
    Posted on April 25, 2017 at 03:14

    Thanks Clive One. 

    L C
    L CAuthor
    Associate III
    April 29, 2017
    Posted on April 29, 2017 at 11:37

    Hi ALL

    with ILI9341 it has command & data information via SPI interface.

    Are they using same SPI function(push data) and necessary to handle the D/C(Data/Command) pin by myself?

    In ILI9341 data sheet, there have 9-bit interface.

    I think it like I2C style, one more bit indicate the following data either data or command.

    Shall we implement it in STM32?

    Please let me know your comment.

    LC

    ________________

    Attachments :

    ILI9341.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hygv&d=%2Fa%2F0X0000000bAz%2FcixjhTg0VdSF3Ynh8TvFjjxpjNRiGkPKjCJBO8XIJFA&asPdf=false
    S.Ma
    Principal
    April 29, 2017
    Posted on April 29, 2017 at 12:28

    There should be also a 8 bit with dedicated pin for command/data.

    For STM32F103, the HW supports 8 or 16 bit bitblock transfer. Extra bit done by SW bit banging?

    For newer STM32 with FIFO'd SPI, the HW supports 4,5,6...16 bits so the 9 bit mode seems a better fit, and save a pin.