Skip to main content
jpb
Visitor II
September 21, 2012
Question

STM32F103 GPIO Output Speed

  • September 21, 2012
  • 1 reply
  • 713 views
Posted on September 21, 2012 at 15:07

When I program a GPIO pin, I have to define a ''speed'': 2, 10 or 50MHz. What does this mean in terms of hardware? Is this a filter?

If I program the pin with 2MHz I can't output a signal with 5MHz. What is the hardware implemented in the port circuit that cuts (filter) the output signal frequency?

Thank you
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    September 21, 2012
    Posted on September 21, 2012 at 16:04

    It relates to the slew control on the pin, and defines how sharp the rising/falling edges are, and how hard/rapidly the pin is driven.

    Define it too slow, and your output waveform will be less square, will depend on the capacitive load being driven. Drive it too hard, you tend to get under/over shoot, which will also add to the EMI generated.

    Generally you'd want to set it appropriately for the signal being output.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..