Skip to main content
bharatig154
Associate III
January 7, 2016
Question

stm32f103 firmware upgrade remotely possible or not

  • January 7, 2016
  • 11 replies
  • 3345 views
Posted on January 07, 2016 at 11:05

How to upgrade firmware of stm32f103 controller using over the air programming?

    This topic has been closed for replies.

    11 replies

    Tesla DeLorean
    Guru
    January 7, 2016
    Posted on January 07, 2016 at 11:19

    Four threads?

    Suggest you review the IAP (In Application Programming) examples for your part. Build yourself a small loader that uses your specific type of 'Air' to transfer the data, and erase and write blocks of flash with this new data.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bharatig154
    Associate III
    February 18, 2016
    Posted on February 18, 2016 at 05:57

    Hi

    can anybody tell me how to download a bin file to controller stm32f103rb through gsm for IAP purpose

    Tesla DeLorean
    Guru
    February 18, 2016
    Posted on February 18, 2016 at 14:52

    You'd want to look at using FTP or HTTP to connect to your file server, the modem may have high level functions to do this, or socket commands you can use to implement them.

    Ideally your platform should have a place to stage the firmware image, like an SD Card, or NAND, from which you can copy and update the part using a smaller loader. The alternative is to have a larger loader capable of doing the file transfer and writing the memory directly. This requires strong flow control as the processor will stall if you attempt to execute and write using the internal flash.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bharatig154
    Associate III
    February 19, 2016
    Posted on February 19, 2016 at 05:48

    do you have some sample code so I can understand the concept.

    Tesla DeLorean
    Guru
    February 19, 2016
    Posted on February 19, 2016 at 12:38

    do you have some sample code so I can understand the concept.

    I think you are confusing concept and implementation, ie what you need to implement vs how you're going to do it. I'm not looking to do your job here, so think of a number and sending it to me.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bharatig154
    Associate III
    February 19, 2016
    Posted on February 19, 2016 at 13:25

    Also I want some idea for downloading a code from external eeprom to stm32f103 using y modem protocol

    Tesla DeLorean
    Guru
    February 19, 2016
    Posted on February 19, 2016 at 18:01

    Yeah, I'm not thinking you need Y-Modem to do that, just routines to access your binary image in a linear fashion. Just like you'd read blocks from a file, you have a stream of binary data that represents the image you want to transfer to Internal Flash. You'd perhaps want to structure the stream so it infers length, and a checksum for integrity.

    For the F4-DISCOs there were some ''FW Upgrade'' examples in the SPL releases where it would pull a file from a USB attached Flash Drive and write that into memory. I've built similar things with SD Cards, where I've taken the SDIO driver, FatFs, and some Flash Erase/Write routines to update my application space.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bharatig154
    Associate III
    February 20, 2016
    Posted on February 20, 2016 at 10:28

    Thanx

    bharatig154
    Associate III
    February 25, 2016
    Posted on February 25, 2016 at 12:29

    Hi all,

    I'm working on SIM900 module to upload data to server ,

    i'm using AT command set to upload data through GSM modem...

    when i''m trying to upload data through termnal manually it's working fine....

    when i'm trying to use the same procedure and flow to develep a firm ware(for STM32 controller)

    it's not working fine....

    i'm getting error for two commands...

    AT+SAPBR=1,1... for this command some time i'm getting response as OK and some times ERROR... 

    after getting ERROR when i retry the same command multiple times it's giving same responce....

    AT+FTPPUT=1... for this command i'm getting responce OK followed by +FTPPUT=1,1,1360.. normally... but many times i'm getting +FTPPUT=1,61 (or)

    +FTPPUT=1,77 (or)+FTPPUT=1,72 many times..... after gettingthis error i've tried many time to up load data through controller it's giving same error responce.....

    Is there any solution for this.......

    thankYou......

    Tesla DeLorean
    Guru
    February 25, 2016
    Posted on February 25, 2016 at 22:09

    Does your automated code wait for the SIM to be read, and the modem register on the network? Do you check the registration state, and activate a context?

    I don't have a SIM900, so not going to be much help walking you through its behaviour.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..