Skip to main content
bsy006
Associate II
January 15, 2009
Question

STM32F103 BootLoader Go command

Posted on January 15, 2009 at 13:39

STM32F103 BootLoader Go command

    This topic has been closed for replies.

    3 replies

    bsy006
    bsy006Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    Hello, I'm using STM32F103, have a problem to start go RAM downloaded code.

    Connect by serial. Read memory, Download, all other commands to BootLoader work OK - reply as explained in AN2606.

    After 'go' command, it doesn't look it starts. I try to download easiest code (40 bytes) which should change memory, so I could then see the result,

    but nothing happens.

    'Go' command returns ACK 2 times, after command itself, and after address.

    BootLoader v 2.0.

    [ This message was edited by: YuSh on 13-01-2009 19:31 ]

    johan239955_st
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    I can just say that I've had the same problems. However, for me it works for some applications but not for others.

    The applications that I can't start from the bootloader, works if I reset the device and boot from flash instead...

    Is this a documented bug, or are we doing something wrong?

    bsy006
    bsy006Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    Hi, Johan,

    could you tell me what is the code you succeded to start from RAM, by BL 'GO' command ?

    Till now, I had no code, even easiest, gives sign of starting to run.

    If you have some code do start, it may help to understand the problem.

    With regards,

    Yuri.