Skip to main content
vaclav23
Associate II
October 13, 2011
Question

STM32F103 and TIM3 and DMA - how to?

  • October 13, 2011
  • 1 reply
  • 1049 views
Posted on October 13, 2011 at 13:58

Hello all,

I have linebuffer[256] and want to quickly send it to GPIOB15-8. In TIM2_IRQ, I enable DMA and TIM3 is used for DMA requests. I am trying following configuration:

   RCC->APB1ENR = RCC_APB1ENR_TIM2EN | RCC_APB1ENR_TIM2EN ; // enable TIM2 and TIM3

   RCC->AHBENR = RCC_AHBENR_DMA1EN; // enable DMA1

   // config of TIM3 - for DMA

   TIM3->ARR = 5;

   TIM3->PSC = 0;   // f=72MHz, ARR=5, PSC=0 => fpixclk = 12MHz

   TIM3->SMCR = 0;

   TIM3->DIER = TIM_DIER_UDE; // DMA request enable

   TIM3->CR2 = 0;

   TIM3->CR1 = TIM_CR1_URS | TIM_CR1_CEN;

   // config of DMA1 channel3 - TIM3_UP

   DMA1_Channel3->CCR = 0x00003090;

   DMA1_Channel3->CNDTR = 0x100; // 255 bytes

   DMA1_Channel3->CPAR = ((unsigned char)&(GPIOB->ODR))+1;

   DMA1_Channel3->CMAR = (unsigned char ) linebuffer;

   DMA1_Channel3->CCR = 0x00003091;

I assume that each TIM3_UP causes copying of one byte from linebuffer[] to GPIOB15-8. When 256 bytes is transferred, DMA stops and waits for reconfiguration in TIM2_IRQ.

I noticed that TIM3 has DCR and DMAR registers. But I don't know at all, what they are good for. They seem to me that they are not used in DMA controller but just to self-update.

Can anybody help ?

#dma-timer
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
October 13, 2011
Posted on October 13, 2011 at 16:51

Can anybody help ?

Probably, what are you offering?

I'd avoid register level programming the part, and I suspect 12 MHz is going to get pretty close to saturating the bus.

How does this burst of data get latched externally, or are you trying to dump data to a logic analyser, or a scope trace? Do you plan to clock externally using a TIM output?

Wouldn't shoveling out via an external bus (FSMC) in a memory-to-memory DMA, or Memory-to-GPIO DMA be more effective than using the timer at all?
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..