Question
stm32f100r8 external interrupt
Posted on April 11, 2018 at 08:09
Hi friends,
I am using stm32f100r8 with standart peripheral driver.
I have planned to use porta1, porta6, portb2, portb3 and portb4 as an external interrupt pin.
I use same config for all of them.
But portb2 and portb3 can not work as an external interrupt pin.
What can be the problem?
Below example, Portb4 can work but Portb2 can not.
define ZC_PORT GPIOB
#define ZC_GPIO_CLK RCC_APB2Periph_GPIOB#define ZC_PIN_NUM GPIO_Pin_4 // PB4#define ZC_PORT_SOURCE GPIO_PortSourceGPIOB#define ZC_PIN_SOURCE GPIO_PinSource4 #define ZC_EXTI_LINE EXTI_Line4 // EXTI Line4#define ZC_EXTI_IRQ EXTI4_IRQn // EXTI4 IRQ#define TRIP18V_PORT GPIOB
#define TRIP18V_GPIO_CLK RCC_APB2Periph_GPIOB#define TRIP18V_PIN_NUM GPIO_Pin_2 #define TRIP18V_PORT_SOURCE GPIO_PortSourceGPIOB#define TRIP18V_PIN_SOURCE GPIO_PinSource2 #define TRIP18V_EXTI_LINE EXTI_Line2 #define TRIP18V_EXTI_IRQ EXTI2_IRQnRCC_APB2PeriphClockCmd(ZC_GPIO_CLK, ENABLE);
GPIO_InitStructure.GPIO_Pin = ZC_PIN_NUM; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(ZC_PORT, &GPIO_InitStructure); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); GPIO_EXTILineConfig(ZC_PORT_SOURCE, ZC_PIN_SOURCE); RCC_APB2PeriphClockCmd(TRIP18V_GPIO_CLK, ENABLE); GPIO_InitStructure.GPIO_Pin = TRIP18V_PIN_NUM; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(TRIP18V_PORT, &GPIO_InitStructure); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); GPIO_EXTILineConfig(TRIP18V_PORT_SOURCE, TRIP18V_PIN_SOURCE);EXTI_InitStructure.EXTI_Line = ZC_EXTI_LINE;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); EXTI_InitStructure.EXTI_Line = TRIP18V_EXTI_LINE; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure);NVIC_InitStructure.NVIC_IRQChannel = ZC_EXTI_IRQ;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 4; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = TRIP18V_EXTI_IRQ; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 4; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);