Question
STM32f100: empty project for IAR Embedded Workbench
Posted on June 21, 2011 at 18:21
Hi, I have to create a firmware using stm32f100 microcontroller.
I don't be able to start because the project that i use doesn't function. I need someone that is working, or he has morked whit this micro and with this program and can send me the project file structure by email. I would use the STM32F10x_StdPeriph_Lib_V3.5.0. Thank you!! #microcontroller-projects #firmware-library #stm32