Skip to main content
asrock70
Associate III
October 23, 2015
Question

STM32F1 v2.0.0 SW pack for MDK-ARM, STM32CubeMX?

  • October 23, 2015
  • 2 replies
  • 950 views
Posted on October 23, 2015 at 10:06

I installed

Software Pck for STM32F1 v2.0.0 to my MDK-ARM v5.16a, create project for STM32F103RB, add support for device SPI, in RTE_DEvice.h select SPI1, but when compule have eeror C:\Keil\ARM\PACK\Keil\STM32F1xx_DFP\2.0.0\RTE_Driver\SPI_STM32F10x.c(316): error: #20: identifier ''RCC_APB1RSTR_SPI3RST'' is undefined

if (spi == SPI1) { RCC->APB2RSTR |= RCC_APB2RSTR_SPI1RST; } 
else if (spi == SPI2) { RCC->APB1RSTR |= RCC_APB1RSTR_SPI2RST; } 
else if (spi == SPI3) { RCC->APB1RSTR |= RCC_APB1RSTR_SPI3RST; }

a

software developer

at

ST

unaware that

low and medium density STM32F1 MCU

do not have

SPI3?

Can

somewhere

report

found

bugs in software

pack ?

Second question. STM32CubeMX generate project for MDK-ARM v5 , Firmware Package v1.2 include own HAL driven own support for FreeRTOS, Software packt v2.0.0 for MDK-ARM support

another owner

HAL driver, support fro RTX .

It is

written

somewhere

how

these things

integrated

and

used in the

same project?

    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    November 18, 2015
    Posted on November 18, 2015 at 14:55

    Hi Charles,

    Thank you for your feedback. The issue has been reported internally.

    -Syrine-

    stm32cube-t
    ST Employee
    November 25, 2015
    Posted on November 25, 2015 at 19:03

    Dear user,

    On smaller packages some peripherals are not available. It is the case here with SPI3.

    Regarding the project generation flow, you use STM32CubeMX to select your MCU, perform your configuration (including the toolchain you want to generate your project for).

    STM32CubeMX will automatically propose the download of the necessary STM32Cube Libraries. Within MDK-ARM IDE, you may have to install the device pack support the MCU you selected.

    For now, STM32Cube supports only freeRTOS so for RTX you will have to manually update your project within the IDE itself.

    Best regards