Question
STM32F1/F4 incompatible I/O
Posted on December 08, 2011 at 19:34
From their respective RMs:
STM32F1... 0x4002 2000 - 0x4002 23FF Flash memory interface STM32F4... 0x4002 2000 - 0x4002 23FF GPIOI Thus a project predicated on STM32x compatibility must have at least different I/O base addresses based on processor type. Damn! I guess I have to say it again, “substantial compatibility� or in ST’s case, “compatible�, means incompatible. Now I have to go through, identify all the differences and come up with a way to select the proper include files. Does anyone know if the (possibly subset of) I/O offset address are always the same?