Skip to main content
PPete.11
Associate
May 11, 2020
Question

STM32F091RC-Nucleo BSP (Board Support Package) Execution Instruction!

  • May 11, 2020
  • 0 replies
  • 988 views

This passage is forwarded from RT-Thread IoTOS Twitter. FYI: RT-Thread is an open-source real-time operating system(RTOS)

You can reach out the original article on https://hashnode.com/post/stm32f091rc-nucleo-bsp-board-support-package-execution-instruction-ck9me97yy001pihs1pfi7evk0

The mainly-used resources of this board are shown as follows:

  • MCU: STM32F091, Main Frequency 48MHz, 256KB FLASH, 32KB RAM
  • External RAM: None
  • External FLASH: None
  • Common peripherals -Button: one, user (has the wake-up feature, PC13)
  • Common-used interfaces: USB, Arduino interface, etc.
  • Debug interface: standard SWD For more details about this board, please refer to ST official.

Peripheral Condition

Each peripheral supporting condition for this BSP is as follows:

0693W000000XAVjQAO.png

Instruction

-Get started

This BSP provides MDK4, MDK5, and IAR projects for developers and it supports the GCC development environment. Here's an example of the MDK5 development environment, to introduce how to run the system.

-Hardware connection

Use a USB cable to connect the development board to the PC and turn on the power switch.

-Compile and Download

Double-click the project.uvprojx file, to open the MDK5 project, compile and download the project to the board.

By default, the executable file will be downloaded to the board by the simulator, which is connected to PC via the USB cable.

-Running Results

Once the project is successfully downloaded, the system runs automatically.

Connect the serial port of the board to PC, communicate with it via a serial terminal tool (115200bps, 8N1). Restart the board and the startup information of RT-Thread will be observed:

 \ | /
 
- RT - Thread Operating System
 
 / | \ 4.0.0 build Dec 21 2018
 
 2006 - 2018 Copyright by rt-thread team
 
msh >
 

Advanced Features

This BSP only enables GPIO and serial port 2 by default. If you need more advanced features such as SPI, I2C, you need to configure the BSP with ENV tools, as follows:

  1. Open the env tool under BSP.
  2. Enter menuconfig command to configure the project, then save and exit.
  3. Enter pkgs --update command to update the package.
  4. Enter scons --target=mdk4/mdk5/iar command to regenerate the project.

This topic has been closed for replies.