Skip to main content
Rick1
Associate II
Nov 10, 2020 4:36 PM UTC
Solved

STM32F091CCT6: Why my led doesn't blink?

Hi there.

I have a board from some equipament which has a STM32F091CCT6 uC, and there are 3 leds, connected to pin GPIO_C13, GPIO_C14 and GPIO_A7. Anode from leds are connected to Vcc and Catode are connected in a resistor and then to the uC pins (so it turns ON when pin is low).

I set up everything with the configuration tool from STM32cubeIDE, so it made all the code for me, which you can see below. But I've already tried a lot of different code to blink my led, any of them, but none will blink! I can turn them on OR off, but blink...never.

Does anyone know what's wrong with the code? thanks

#include "main.h"
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
 
int main(void)
{
 HAL_Init();
 MX_GPIO_Init();
 while (1)
 {
 /* USER CODE END WHILE */
	 HAL_GPIO_WritePin(GPIOC,GPIO_PIN_14,GPIO_PIN_RESET);
	 HAL_Delay(1000);
	 HAL_GPIO_WritePin(GPIOC,GPIO_PIN_14,GPIO_PIN_SET);
	 HAL_Delay(1000);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13|GPIO_PIN_14, GPIO_PIN_RESET);
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2|GPIO_PIN_7, GPIO_PIN_RESET);
 
 /*Configure GPIO pins : PC13 PC14 */
 GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_14;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
 /*Configure GPIO pins : PA2 PA7 */
 GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_7;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

in Main, I have already tried this, but it I didn't succeed

 while (1)
 {
 /* USER CODE END WHILE */
	 HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_14);
	 HAL_Delay(1000);
 /* USER CODE BEGIN 3 */
 }

This topic has been closed for replies.
Rick1
Rick1Best answer
Associate II
Nov 11, 2020 8:43 PM UTC

Thanks.

This board I was using had some weird circuit which was reseting my uC.

Now it blinks beautifully!

3 replies

TDK
Nov 10, 2020 6:37 PM UTC

Your code looks fine.

Test the LEDs with a multimeter in diode mode to ensure they work and are wired correctly.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Rick1
Rick1AuthorBest answer
Associate II
Nov 11, 2020 8:43 PM UTC

Thanks.

This board I was using had some weird circuit which was reseting my uC.

Now it blinks beautifully!

ST Technical Moderator
Nov 11, 2020 8:34 PM UTC

Hello @Rick​ ,

I recommend you to follow step-by-step Blink led tutorial, this help you on your application to blink a led.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks