STM32F072RB interfacing with nrf24l01
- December 2, 2020
- 0 replies
- 675 views
I am using STM32F072RB and I have interfaced it with NRF24L01 module.
I have refer the library files attached below for nrf24l01 module.
I am trying to send string "Hello World" from one module to another. .Transmission found ok, but at receiving side I didn't get the result...
NRF24_available() result is not getting true...
Can anyone help me to get out of this stuff...
code flow as below :
NRF24_begin(GPIOA, CSN_Pin, CE_Pin, hspi1);
nrf24_DebugUART_Init(huart1);
NRF24_setAutoAck(false);
NRF24_setChannel(52);
NRF24_setPayloadSize(32);
NRF24_openReadingPipe(1, RxpipeAddrs);
NRF24_startListening();
while (1)
{
if(NRF24_available())
{
NRF24_read(myRxData, 32);
myRxData[32] = '\r';myRxData[32+1] = '\n';
HAL_UART_Transmit(&huart1, (uint8_t*)myRxData, 32+2, 50);
}
}