Skip to main content
abotha
Associate III
Jan 16, 2017 10:41 AM UTC
Solved

STM32F072RB Comparator to Timer2 Frequency Counter

Posted on January 16, 2017 at 11:41

Good Day

I have an oscillator connected to Comparator 1, I want the output of Comparator 1 to internally go to timer 2.

I would like to manually start TIM2, leave it for a few milliseconds, and come back and read how many times the comparator changed state. I then want to reset the value back to zero and it must start counting up again, one count for every transition of the from high to low on the comparator.

How must I set up timer 2 to achieve this? I have it set-up as Slave Mode with External Input but I think it is incorrect.

I have set Comparator 1 as follows:

void MX_COMP1_Init(void){
hcomp1.Instance = COMP1; 
hcomp1.Init.InvertingInput = COMP_INVERTINGINPUT_IO1; 
hcomp1.Init.NonInvertingInput = COMP_NONINVERTINGINPUT_IO1; 
hcomp1.Init.Output = COMP_OUTPUT_TIM2IC4; 
hcomp1.Init.OutputPol = COMP_OUTPUTPOL_NONINVERTED; 
hcomp1.Init.Hysteresis = COMP_HYSTERESIS_LOW; 
hcomp1.Init.Mode = COMP_MODE_HIGHSPEED; 
hcomp1.Init.WindowMode = COMP_WINDOWMODE_DISABLE; 
hcomp1.Init.TriggerMode = COMP_TRIGGERMODE_IT_RISING; 
if (HAL_COMP_Init(&hcomp1) != HAL_OK) 
{ Error_Handler(); }
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?

and Timer 2 like this:

/* TIM2 init function */
void MX_TIM2_Init(void)
{
 TIM_SlaveConfigTypeDef sSlaveConfig;
 TIM_MasterConfigTypeDef sMasterConfig;
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 150000;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sSlaveConfig.SlaveMode = TIM_SLAVEMODE_EXTERNAL1;
 sSlaveConfig.InputTrigger = TIM_TS_TI1F_ED;
 sSlaveConfig.TriggerFilter = 5;
 if (HAL_TIM_SlaveConfigSynchronization(&htim2, &sSlaveConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

#timer-channels #stm32f072 #comparator #timer #input-capture
This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Jan 16, 2017 12:53 PM UTC
Posted on January 16, 2017 at 12:53

Look at the TIMx_SMCR.TS description in RM: from the channels (inputs) of the given timer, only TI1FP1 and TI2FP2 can be used as TRGI (thus subsequently as source for external clock mode 1).

JW

4 replies

waclawek.jan
Super User
Jan 16, 2017 11:02 AM UTC
Posted on January 16, 2017 at 12:02

The comparator is connected to Input Capture 4 (i.e. Channel 4) which can't be used as external clock.

Why don't you use the TIM1/IC1 or TIM3/IC1 connection?

JW

abotha
abothaAuthor
Associate III
Jan 16, 2017 12:27 PM UTC
Posted on January 16, 2017 at 12:27

Hi JW, what would be different changing from one Input Capture to another?

Is that the mode that I should be on to achieve what I described (counting pulses in a given time period)?

waclawek.jan
waclawek.janBest answer
Super User
Jan 16, 2017 12:53 PM UTC
Posted on January 16, 2017 at 12:53

Look at the TIMx_SMCR.TS description in RM: from the channels (inputs) of the given timer, only TI1FP1 and TI2FP2 can be used as TRGI (thus subsequently as source for external clock mode 1).

JW