Skip to main content
pfischer
Visitor II
April 17, 2015
Question

STM32F072CBT6 Reset

  • April 17, 2015
  • 0 replies
  • 527 views
Posted on April 17, 2015 at 10:48

Hi there

I designed a print with a STM32F072CBT6 and connect with a Discovery Board.

First I designed the software on the Discovery Board. After that, i want to test the connection to the CBT6. My Code works fine on the first try but after disconnect, the mcu starts itself after 5ms, repeating itself and i cant connect with to stop an reprogram it. Is there a way to force the chip to reset/flash the rom?

My IDE is the free version of Keil

My Startup Code:

/* Includes ------------------------------------------------------------------*/

&sharpinclude ''stm32f0xx_hal.h''

/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart1;

DMA_HandleTypeDef hdma_usart1_rx;

DMA_HandleTypeDef hdma_usart1_tx;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_DMA_Init(void);

static void MX_USART1_UART_Init(void);

/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

int main(void)

{

  /* USER CODE BEGIN 1 */

    uint8_t aTransmitBuffer[3];

    aTransmitBuffer[0]=0x55;

    aTransmitBuffer[1]=0xFF;

    aTransmitBuffer[2]=0x32;

  /* USER CODE END 1 */

  /* MCU Configuration----------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

  HAL_Init();

  /* Configure the system clock */

  SystemClock_Config();

  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  MX_DMA_Init();

  MX_USART1_UART_Init();

  /* USER CODE BEGIN 2 */

  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);

  HAL_UART_Transmit_DMA(&huart1, &aTransmitBuffer[0], 3);

  /* USER CODE END 2 */

  /* USER CODE BEGIN 3 */

  /* Infinite loop */

  while (1)

  {

  }

  /* USER CODE END 3 */

}

#external-reset
    This topic has been closed for replies.