Skip to main content
Handzic.Dirk
Associate III
Jan 9, 2019 9:46 AM UTC
Solved

STM32F071C PLL never gets ready on some boards

I have a problem on a STM32F071C board. The PLL will not reach ready state. I am using the HSI and in order to reduce current consumption I want to devide PLL from 8MHz down to 2MHz. This works fine on most board (18 out of 20) but on some the PLL_RDY is never set. Do I violate any requirements by using RCC->CFGR2 = RCC_CFGR2_PREDIV_DIV4?

   

/* Enable Prefetch Buffer and set Flash Latency */

   FLASH->ACR = FLASH_ACR_PRFTBE | FLASH_ACR_LATENCY;

   /* HCLK = SYSCLK */

   RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1;

   /* PCLK = HCLK */

   RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE_DIV1;

   /* PLL configuration = HSI * 2 = 4 MHz */

   RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLXTPRE | RCC_CFGR_PLLMUL));

   RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSI_PREDIV | RCC_CFGR_PLLMUL2);

   RCC->CFGR2 = RCC_CFGR2_PREDIV_DIV4;

   /* Enable PLL */

   RCC->CR |= RCC_CR_PLLON;

   /* Wait till PLL is ready */

   while((RCC->CR & RCC_CR_PLLRDY) == 0)

   {

   }

   /* Select PLL as system clock source */

   RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW));

   RCC->CFGR |= (uint32_t)RCC_CFGR_SW_PLL;   

   /* Wait till PLL is used as system clock source */

   while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_PLL)

   {

   }

This topic has been closed for replies.
Danish1
Danish1Best answer
Lead III
Jan 9, 2019 11:31 AM UTC

As a comment, I don't like the way you modify RCC->CFGR, doing it in two hits with the first to clear some bits and the second to set others.

Looking at the data sheet section 6.3.9, I think the PLL should be able to sing between 16 and 48 MHz. So maybe getting the PLL to run at 8 MHz is outside the specification, and you have to run it at 16 MHz and divide by 2 (or whatever you want) to get HCLK.

Hope this helps,

Danish

4 replies

Danish1
Danish1Best answer
Lead III
Jan 9, 2019 11:31 AM UTC

As a comment, I don't like the way you modify RCC->CFGR, doing it in two hits with the first to clear some bits and the second to set others.

Looking at the data sheet section 6.3.9, I think the PLL should be able to sing between 16 and 48 MHz. So maybe getting the PLL to run at 8 MHz is outside the specification, and you have to run it at 16 MHz and divide by 2 (or whatever you want) to get HCLK.

Hope this helps,

Danish

Handzic.Dirk
Associate III
Jan 9, 2019 12:11 PM UTC

You are right, I only checked the PLL input frequency which is ok down to 1 MHz but the min output frequency is 16 MHz. That is probably the problem.

Thanks!

Uwe Bonnes
Chief
Jan 9, 2019 1:38 PM UTC

Why do you need PLL at all? Use HSI16 with AHB Prescaler 2 to get 8 MHz.

Handzic.Dirk
Associate III
Jan 9, 2019 2:47 PM UTC

I am now running directly out of the HSI8 and PLL turned off. Problem solved!