STM32F070CBT6 SysTick_Handler never called
- 2 replies
- 1059 views
Hi all,
I have a custom board I have designed with an STM32F070CBT6 on it. Currently it is only populated with the power regulator, one led hooked up to pin PA1 and the debug header.
I've used STM32CubeMX to generate a simple test project that initialises the SysTick timebase source, and GPIO on pin PA1. It is clocked using the internal HSI RC oscillator at 8Mhz.
When I build and debug the project using SW4STM32 the debugger steps over HAL_Init(), SystemClock_Config(), and MX_GPIO_Init() successfully, but hangs shortly after that. E.g. if I put the following in the main() while loop:
while (1)
{
HAL_GPIO_TogglePin(STATUS_LED_GPIO_Port, STATUS_LED_Pin);
HAL_Delay(500);
}It will step over the call to HAL_GPIO_TogglePin succesfully turning on the LED, but then hangs at HAL_Delay(500);
If I put a breakpoint in the SysTick_Handler(void) function in stm32f0xx_it.c it never gets hit. It appears like the interrupts aren't firing.
I've attached my CubeMX project file in case that is of help understanding why this might not be working. With the exception of lines 3 & 4 in the code snippet above the rest of the project is vanilla generated code.
Thanks very much for any advice you can provide!
Cheers,
James Fitzsimons