Associate II
May 14, 2014
Question
STM32F05x SPI clk single bit
- May 14, 2014
- 4 replies
- 1284 views
Posted on May 14, 2014 at 17:07
Hi,
I have a PCB with a STM32F051 connected to 3 ADCs (http://datasheets.maximintegrated.com/en/ds/MAX11166-MAX11pdf
) in daisy chain. Page 29 Figure 14 of the datasheetshows the schematic I implemented andPage 21 shows how to configure the chips.... My problem is (page 21): ''The load process is enabled on the falling edge ofCNVST when SCLK is held high. '' The SPI is normally in LowPolarity and Falling Edge, But in order to create the situation above I switch on the fly the polarity and Edge of the system to get the CLK high while CNVST falls... (I attached a screenshot...) Very dirty way.. and I'm not sure if the ADCs are not upset by the extra clk falling edge at the end of the communication when I go back to the normal polarity.void
ADCs_init(
void
)
{
uint16_t tmpreg = 0;
SPI_Cmd(SPI1, DISABLE);
tmpreg = SPI1->CR1;
tmpreg &= 0xFFFC;
tmpreg |= (SPI_CPHA_1Edge | SPI_CPOL_High);
SPI1->CR1 = tmpreg ;
/* Write to SPIx CR1 */
GPIO_SetBits(ADC_CNVST_PORT,ADC_CNVST_PIN);
SPI_Cmd(SPI1, ENABLE);
GPIO_ResetBits(ADC_CNVST_PORT,ADC_CNVST_PIN);
/* Drop CNVST to enable the load process */
Send_Receive_Byte(0xC0);
// Daisy Chain Mode with busy indicator, Reference mode 0, Normal mode.
Send_Receive_Byte(0xC0);
// Daisy Chain Mode with busy indicator, Reference mode 0, Normal mode.
Send_Receive_Byte(0xC0);
// Daisy Chain Mode with busy indicator, Reference mode 0, Normal mode.
GPIO_SetBits(ADC_CNVST_PORT,ADC_CNVST_PIN);
SPI_Cmd(SPI1, DISABLE);
tmpreg = SPI1->CR1;
tmpreg &= 0xFFFC;
tmpreg |= (SPI_CPHA_2Edge | SPI_CPOL_Low);
SPI1->CR1 = tmpreg ;
/* Write to SPIx CR1 */
SPI_Cmd(SPI1, ENABLE);
}
uint8_t Send_Receive_Byte(uint8_t byte)
{
/*!< Send byte through the SPI1 peripheral */
SPI_SendData8(SPI1, byte);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET);
/*!< Return the byte read from the SPI bus */
return
SPI_ReceiveData8(SPI1);
}
Do you know a nice way to control the CLK level?
Thanks,
Alex