Skip to main content
paulkinzer9
Associate II
Dec 12, 2016 2:00 PM UTC
Solved

STM32F051R8T6 pin compatible with STM32F091RCT6?

Posted on December 12, 2016 at 15:00

I'm currently using the STM32F051R8T6, 64 pin LQFP.  Is the STM32F091RCT6 in the same package fully pin-compatible?

Thanks,

Paul♯♯♯

#stm32f091 #compatible #stm32f051
This topic has been closed for replies.
Lawliet KG
Lawliet KGBest answer
Visitor II
Dec 12, 2016 8:55 PM UTC
Posted on December 12, 2016 at 21:55

Hi Paul,

No, those two products are not fully pin to pin compatible.

I advise you to download their datasheets and see the pinout differences on section 'Pinouts and pin descriptions'.

Best regards,

Lawliet.

If this answers your request, please press 'correct' 

:)

.

3 replies

Lawliet KG
Lawliet KGBest answer
Visitor II
Dec 12, 2016 8:55 PM UTC
Posted on December 12, 2016 at 21:55

Hi Paul,

No, those two products are not fully pin to pin compatible.

I advise you to download their datasheets and see the pinout differences on section 'Pinouts and pin descriptions'.

Best regards,

Lawliet.

If this answers your request, please press 'correct' 

:)

.
paulkinzer9
Associate II
Dec 13, 2016 2:37 PM UTC
Posted on December 13, 2016 at 14:37

Thanks.  I looked at the pinout of the package I need, and found that they're close.  PF5, PF6, PF7 are VSS/VDD pins on the '091.  I only use Ports A/B/C, so with a simple board change, I can switch to this part, and get 4x the RAM.  That should work out just fine.

Lawliet KG
Visitor II
Dec 13, 2016 3:55 PM UTC
Posted on December 13, 2016 at 15:55

Hi Paul,

Do not forget to connect the new VDD/VDDIO2/VSS pins.

And, your migtation to STM32F091 should be fine.

Regards,

Lawliet.