Question
STM32F051R8 missing interrupt response
Posted on December 16, 2012 at 14:20
During programming trials on a STM32F051 discovery cardlet I found out that the TIM1 update interrupt does not work while using TIM1 channel 4 for PWM input signal evaluation. The update flag UIF is set, but no interrupt happens. Other interrupt events of TIM1 function correcly. I circumvented that problem by using the compare feature of a free channel of TIM1. Is this missing interrupt a design problem or a single failure on my specific chip?
Any help is appreciated. Here are the specific F051 chip data: STM32F051 R8T6 GH221 W6 CHN GH 207 #stm32f051 #tim1 #uif