Skip to main content
wb0gaz
Associate III
February 1, 2022
Solved

STM32F051 TIM6 "basic" - more registers defined in STM32F051x8.h than RM0091 TIM6 section

Beginning to explore timers in STM32F051 (from DiscoveryF0). I'm starting with TIM6 (basic timer) as I'm looking for nothing more than a periodic interrupt. Before I get started, I'm wrestling with where to find complete register reference for the component (I plan to interact with timers at register level, bit-by-bit, to learn in detail.)

Datasheet for STM32F051 says

3.14.3 Basic timer TIM6

This timer is mainly used for DAC trigger generation. It can also be used as a generic 16-bit time base.

(I'm not concerned about DAC trigger, just wanted a generic timer.)

RM0091 Section 21,Table76 page 559 defines 8 registers as follows (offsets and names shown below)

0x00 TIMx_CR1

0x04 TIMx_CR2

0x0C TIMx_DIER

0x10 TIMx_SR

0x14 TIMx_EGR

0x24 TIMx_CNT

0x28 TIMx_PSC

0x2C TIMx_ARR

STM32F051x8.h (in Drivers/CMSIS/Device/ST/STM32F0xx/Include/) defines the register structure for TIM6 using a template (TIM_TypeDef) that appears to be common to many (most? all?) timers, which is why I'm asking my question:

(line 591 of STM32F051x8.h)

#define TIM6               ((TIM_TypeDef *) TIM6_BASE)

This refers to a structure definition containing 21 register offsets, not 8.

typedef struct

{

 __IO uint32_t CR1;         /*!< TIM control register 1,             Address offset: 0x00 */

 __IO uint32_t CR2;         /*!< TIM control register 2,             Address offset: 0x04 */

 __IO uint32_t SMCR;        /*!< TIM slave Mode Control register,    Address offset: 0x08 */

 __IO uint32_t DIER;        /*!< TIM DMA/interrupt enable register,  Address offset: 0x0C */

 __IO uint32_t SR;          /*!< TIM status register,                Address offset: 0x10 */

 __IO uint32_t EGR;         /*!< TIM event generation register,      Address offset: 0x14 */

 __IO uint32_t CCMR1;       /*!< TIM capture/compare mode register 1, Address offset: 0x18 */

 __IO uint32_t CCMR2;       /*!< TIM capture/compare mode register 2, Address offset: 0x1C */

 __IO uint32_t CCER;        /*!< TIM capture/compare enable register, Address offset: 0x20 */

 __IO uint32_t CNT;         /*!< TIM counter register,               Address offset: 0x24 */

 __IO uint32_t PSC;         /*!< TIM prescaler register,             Address offset: 0x28 */

 __IO uint32_t ARR;         /*!< TIM auto-reload register,           Address offset: 0x2C */

 __IO uint32_t RCR;            /*!< TIM repetition counter register,           Address offset: 0x30 */

 __IO uint32_t CCR1;        /*!< TIM capture/compare register 1,     Address offset: 0x34 */   

 __IO uint32_t CCR2;        /*!< TIM capture/compare register 2,     Address offset: 0x38 */   

 __IO uint32_t CCR3;        /*!< TIM capture/compare register 3,     Address offset: 0x3C */

 __IO uint32_t CCR4;        /*!< TIM capture/compare register 4,     Address offset: 0x40 */

 __IO uint32_t BDTR;           /*!< TIM break and dead-time register,           Address offset: 0x44 */

 __IO uint32_t DCR;         /*!< TIM DMA control register,           Address offset: 0x48 */

 __IO uint32_t DMAR;           /*!< TIM DMA address for full transfer register, Address offset: 0x4C */

 __IO uint32_t OR;          /*!< TIM option register,                Address offset: 0x50 */

} TIM_TypeDef;

To get a complete picture of operating TIM6, should I refer to other timers' definitions for the registers which are not defined in the TIM6 section of RM0091 (section 21) - that is, not rely solely on the definition in section 21?

Is the idea that TIM_TypeDef is common and then each individual timer customizes from there? Does TIM6 incorporate the full register set in TIM_TypeDef?

Thanks for any clarification!

This topic has been closed for replies.
TDK
TDKBest answer
February 2, 2022

> Does TIM6 incorporate the full register set in TIM_TypeDef?

No, it incorporates what is specified in the RM.

TIM_TypeDef is a common structure for all timers and less advanced timers (such as non-advanced timer and basic timers) do not implement everything.

Since other timers are a subset of the advanced ones (except 32 bits in some cases), we're able to use the same structure for all timers which is convenient.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
TDKBest answer
February 2, 2022

> Does TIM6 incorporate the full register set in TIM_TypeDef?

No, it incorporates what is specified in the RM.

TIM_TypeDef is a common structure for all timers and less advanced timers (such as non-advanced timer and basic timers) do not implement everything.

Since other timers are a subset of the advanced ones (except 32 bits in some cases), we're able to use the same structure for all timers which is convenient.

"If you feel a post has answered your question, please click ""Accept as Solution""."
wb0gaz
wb0gazAuthor
Associate III
February 2, 2022

Thank you TDK - that answers my question.

TDK
February 2, 2022

Just as a note, this is similar to both UART and USART peripherals being defined by USART_TypeDef, despite the UART peripherals lacking some of the features.

"If you feel a post has answered your question, please click ""Accept as Solution""."
wb0gaz
wb0gazAuthor
Associate III
February 2, 2022

Thanks very much, TDK!

I greatly appreciate the help you provide in getting me through the learning curve. The structure of the reference manual makes more sense now. I have got TIM6 working properly now, and that will provide a basis to learn the more advanced timers.

Dave