Skip to main content
GBats
Visitor II
July 23, 2019
Question

STM32F042 CAN POLLING WORKS - INTERRUPTS NOT HAPPENING

I have coded it both ways, so the hardware and software works except when switching to interrupt-driven receive. No interrupts happen, though I have checked and rechecked. The global NVIC can interrupt setting is there, and the enable. The CAN priority is set to 1 to allow the SysTick to work for timeouts. The USB interrupt priority is set to 2. I am using all of the snippets in the CAN migration guide from V1 HAL to V2. The transmit always works in polling mode, but I need the receive in interrupt mode. Are there any known quirks about using CAN interrupts on this MPU? Whatever it is seems to be very obscure.

This topic has been closed for replies.