Skip to main content
EFons
Associate II
Apr 23, 2019 5:56 PM UTC
Question

STM32F030R8Tx ADC Problem?

I do not know if and what I am doing wrong. I am using CubeMX and a Nucleo 64-Board. This is the while inside the main:

while (1)
 {
	 if(HAL_ADC_PollForConversion(&hadc, 1000) == HAL_OK){
		 adc_value[i] = HAL_ADC_GetValue(&hadc);
		 media += ((float)adc_value[i++])/n_amostras;
		 r = 0.02*media;
		 v = 0.04*media;
		 comp = 52.91*media;
		 if(i == n_amostras){
		 		 i = 0;
		 		 media = 0;
		 }
	 }
 
 
 }

I do not know if the PollForConversion is the best option, I just used because I saw it in a tutorial in youtube. I need to calculate these values 'r', 'v' and 'comp'. One of my problems is that the ADC is not so accurate as I would like, I would appreciate suggestions about how I could improve this. Also sometimes it does not work as it should, but this could be a problem in my circuit. the values become random, apparently. I will also show the configuration of the ADC:

static void MX_ADC_Init(void)
{
 
 /* USER CODE BEGIN ADC_Init 0 */
 
 /* USER CODE END ADC_Init 0 */
 
 ADC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN ADC_Init 1 */
 
 /* USER CODE END ADC_Init 1 */
 /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) 
 */
 hadc.Instance = ADC1;
 hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc.Init.Resolution = ADC_RESOLUTION_12B;
 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
 hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc.Init.LowPowerAutoWait = DISABLE;
 hadc.Init.LowPowerAutoPowerOff = DISABLE;
 hadc.Init.ContinuousConvMode = ENABLE;
 hadc.Init.DiscontinuousConvMode = DISABLE;
 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc.Init.DMAContinuousRequests = DISABLE;
 hadc.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 if (HAL_ADC_Init(&hadc) != HAL_OK)
 {
 Error_Handler();
 }
 /**Configure for the selected ADC regular channel to be converted. 
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
 sConfig.SamplingTime = ADC_SAMPLETIME_71CYCLES_5;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC_Init 2 */
 HAL_ADCEx_Calibration_Start(&hadc);
 /* USER CODE END ADC_Init 2 */
 
}

I also used the calibration function of the HAL library here, but I do not if I am using it in the right way.

This topic has been closed for replies.

4 replies

Vangelis Fortounas
Associate II
Apr 23, 2019 6:39 PM UTC

Hi

index i , has always the same value. was this your intention?

if i is different than n_amostras then the inside loop "if" statement will never be true.

EFons
EFonsAuthor
Associate II
Apr 24, 2019 11:51 AM UTC

It was not my intention, it is corrected now.

S.Ma
Principal
Apr 23, 2019 7:09 PM UTC

True and also what is the input analog impedence of what is connected... unless there is an external op-amp in follower mode.

Otherwise, ADC result will be lower than expected... and more unstable.

Ozone
Principal
Apr 24, 2019 12:02 PM UTC

Input impedance, S&H capacity and sampling time are interrelated. I guess you know how to deal with it, design-wise.

I suggest to validate the ADC channels first,, by applying known (and different) voltages to all channels, and check the values - either via some output, or in the debugger.