Skip to main content
H.Darwish
Associate II
October 25, 2018
Question

STM32F030K6 stack problem

  • October 25, 2018
  • 4 replies
  • 2131 views

hi

i am trying to make a new project on STM32F030K6 but, after i start and pause debug, a message appears : The stack pointer for stack 'CSTACK' (currently 0x20000658) is outside the stack range (0x20000048 to 0x20000448)  . and the program stuck somewhere.

if i made reset the debugger program (not a hardware reset) , this message will not appears .and the program will run (toggling an LED)

how to solve this .

iam using STM32CUBEMX HAL library , and IAR IDE

thanks in advance

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    October 25, 2018

    >>how to solve this

    Figure out what in your program, or code flow, is causing the stack point to go outside the 1KB (0x400) the linker has assigned to it.

    Any routines using more than 1KB of local/auto variables?

    Check what startup.s is setting the initial stack pointer too, or if it is changing it.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    H.Darwish
    H.DarwishAuthor
    Associate II
    October 25, 2018

    Thank you for you quick reply

    >>Any routines using more than 1KB of local/auto variables? i dont think so ,i am just using one function in my code :HAL_GPIO_TogglePin

    >>Check what startup.s is setting the initial stack pointer too, or if it is changing it.

    actually i am new to STM32 and i dont have experience in startup files but here the part of sp initialization :

     MODULE ?cstartup
     
     ;; Forward declaration of sections.
     SECTION CSTACK:DATA:NOROOT(3)
     
     SECTION .intvec:CODE:NOROOT(2)
     
     EXTERN __iar_program_start
     EXTERN SystemInit
     PUBLIC __vector_table
     
     DATA
    __vector_table
     DCD sfe(CSTACK)
     DCD Reset_Handler ; Reset Handler
     
     DCD NMI_Handler ; NMI Handler
     DCD HardFault_Handler ; Hard Fault Handler
     DCD 0 ; Reserved
     DCD 0 ; Reserved
     DCD 0 ; Reserved
     DCD 0 ; Reserved
     DCD 0 ; Reserved
     DCD 0 ; Reserved
     DCD 0 ; Reserved
     DCD SVC_Handler ; SVCall Handler
     DCD 0 ; Reserved
     DCD 0 ; Reserved
     DCD PendSV_Handler ; PendSV Handler
     DCD SysTick_Handler ; SysTick Handler

    thanks

    Tesla DeLorean
    Guru
    October 25, 2018

    Check in the address assigned for "sfe" in the .MAP file.

    Try to bisect the issue to find out when the SP goes out of range. If it is wrong by the time it hits your main() function, check the SystemInit() function.

    Turn off the "run to main()" functionality in the debugger, and step the code from the Reset_Handler on in.

    >>i am new to STM32

    The STM32 is much like any other ARM Cortex-M micro-controller, and similar in operation to many other micro-controllers in the last 40 or so years.

    IAR is complaining that the SP is outside the scope of the memory it should reside in. This might occur in an RTOS situation where you're allocating stacks to individual tasks, in memory unrelated to the one described by the linker.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    H.Darwish
    H.DarwishAuthor
    Associate II
    October 25, 2018

    HI

    i had found the problem , in my pcb design i was pulling the Boot 0 pin to VCC , so the program was booting from the system memory not from the main flash memory .

    i had connected the boot 0 to vss and unchecked the boot1 in option bytes , and the problem solved :)

    thanks for your help