Skip to main content
guwono.septijo
Associate II
Jan 3, 2014 2:25 PM UTC
Question

STM32F030F4P6 I2C Slave Transmitter Problem : TXI event triggered more times than requested by I2C master

Posted on January 03, 2014 at 15:25

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    5 replies

    guwono.septijo
    Associate II
    Jan 4, 2014 11:41 AM UTC
    Posted on January 04, 2014 at 12:41

    i have a nasty / tricky / stinky solution..

    on flag TXI  :

      ....  bla bla

      if (I2C_GetITStatus(I2C1, I2C_IT_TXIS)) {

          jTX++;

          I2C_ClearITPendingBit(I2C1, I2C_IT_TXI);

          if (jTX > 2) {

             // without this delay below, the byte sent previously was gone !!

             uint16_t delay;

             for (delay = 0; delay < 0x100; delay++) {}

             // brutally kill I2C device and ressurect it

             // maybe not so nasty/stinky because it only

             //   needed to be done once, after MCU's resetted

             I2C_Cmd(I2C1,DISABLE);

             I2C_Cmd(I2C1,ENABLE);

          } else I2C_SendData(I2C1,jTX);

          return 0;

      }

    is it a solution .. or not ? please advice...

    update : it is not a solution. after killing I2C and ressurect it, the I2C becomes screwed !!

    Tesla DeLorean
    Guru
    Jan 4, 2014 2:38 PM UTC
    Posted on January 04, 2014 at 15:38

    You have make a very comprehensive presentation, I'm not much into the F0, CooCox, or I2C, so I'm not sure I can give much advice in those regards.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    guwono.septijo
    Associate II
    Jan 4, 2014 3:17 PM UTC
    Posted on January 04, 2014 at 16:17

    i'm really very glad to see you in my thread, clive1

    i just need a very little advice/info .. :

    => usually we send something using I2C_SendData(I2Cx, Data) in order to suppress TXI interruption....

    my question is : how to CLEAR the TXI flag (Transmit Interrupt) without sending something .. !! ?? !!
    waclawek.jan
    Super User
    Jan 6, 2014 12:34 PM UTC
    Posted on January 06, 2014 at 13:34

    RM0091, Rev4, 24.7.7 (I2Cx_ISR), Bit 1 TXIS: Transmit interrupt status (transmitters)

    [...] Note: This bit is cleared by hardware when PE=0.

    JW
    guwono.septijo
    Associate II
    Jan 6, 2014 4:13 PM UTC
    Posted on January 06, 2014 at 17:13

    From: waclawek.jan

     

    Posted: Monday, January 06, 2014 1:34 PM

     

    Subject: STM32F030F4P6 I2C Slave Transmitter Problem : TXI event triggered more times than requested by I2C master

     

     

    RM0091, Rev4, 24.7.7 (I2Cx_ISR), Bit 1 TXIS: Transmit interrupt status (transmitters)

     

    [...] Note: This bit is cleared by hardware when PE=0.

     

     

    JW

     

     

    thanks JW for your Reply but still no luck...

    I tried it with this :

    I2C1->ISR &= (uint32_t)0xFFFFFFFD;

    CMIIW ...

     

     

    Clear PE flag (Bit 0 of I2C1->CR1 is exactly the same with

     

     

    I2C_Cmd(I2C1,DISABLE);

     

     

    (already in my ''nasty'' solution)

     

     

    Others ?