Question
stm32f030cc how to move application to different location
Posted on August 03, 2015 at 16:25
i am using stm32cube and arm mdk 5 for my code development for stm32f030cc. i developed one free rtos based application which is running fine.i want to develop boot loader to download my rtos based application for remote update using usart.i can not use built in boot loader. so i decide my own bootloader application without free rtos.
i planned that first my boot loader application and then my user application resides in flash.to move my rtos based application to different memory location other than 0x08000000i update start address and length field in (option->target field).but when i download code its not working.so is there is any example or document which help to full fill my need??