Skip to main content
Tim_24
Associate
March 26, 2019
Question

STM32F030CC 48MHz PLL and SysTick...What am I missing?

  • March 26, 2019
  • 3 replies
  • 972 views

Hi,

I'm trying to set the PLL output to 48MHz on a STM32F030CC:

HSI = 8MHz

RCC->CFGR PLLSRC = 0 (PLL input = HSI/2),

PREDIV = not divided.

PLLMUL = 12;

should give (8MHz/2) * 12 = 48MHz but instead I get no clock output on MCO.

Using the MCO output I have confirm the HSI is running, other multiplier factors work fine - I've tried PLLMUL = 10 for example - I would expect (8MHz/2)*10 = 40MHz then MCO divides this by 2 onto the output and I read 20MHz using my scope...works perfectly but not PLLMUL = 12 just a flat line on my scope and no code runs.

If I run the code with the debugger (ST-Link V2, SWDIO/SWCLK connections) it seems to run fine unless I have SysTick interrupt enabled...

Something odd going on, hopefully someone can point me in the right direction?

Thanks,

Tim

This topic has been closed for replies.

3 replies

Tim_24
Tim_24Author
Associate
March 26, 2019

Update on this - It works fine (48MHz PLL) providing HCLK is divided by 4 (RCC_CFGR_HPRE_DIV4) anything less (div by 2/no div) and the code doesn't run.

Is there a limitation to the HCLK speed I am not aware of? The Reference Manual (RM0360) says "The AHB and APB domains maximum frequency is 48MHz" so I should have no problem to set HCLK/PCLK to no div but this is not the case?

Thanks,

Tim

waclawek.jan
Super User
March 27, 2019

If you apply PLL output to HCLK, do you change FLASH latency accordingly?

JW

Tim_24
Tim_24Author
Associate
March 27, 2019

Flash latency set to 1.

Strangely I've tested the same code on other STM32 out of the same 'family' (STM32F030RC, STM32F030R8, STM32F030C8) and not come across the issue - only STM32F030CC.

For now I have HCLK set at DIV4 and PCLK set at no div, then adjusted my timers/SysTick etc.

Tim