Question
STM32F030 first board
Posted on October 28, 2015 at 09:34
Hi to all,
I would like to create my own board using a STM32F030K6T6, but I have some doubts about sending the program from PC to MCU flash. According to datasheet I should tie BOOT0 to '1' and use PA2 and PA3 (USART1) for communication between MCU and PC. In this way if I use an USB to UART adapter such as FT232 I should be able to download my program. Is it right? Second question: which tool can I use to download the program? ST-LINK does not seem to use COM port, so, what can I do? And, at last, how can I set nBOOT1 to '1' if I have not yet programed the MCU? Thank you Freya