Question
STM32F0 Timers
Posted on December 02, 2015 at 00:56
I am having trouble creating a PWM output using a timer (timer 3, channel 1). Processor is an STM32F072CB. I'm using the following code:
Note: GPIO clock is enabled for port ARCC_TypeDef *rccptr = RCC;
// Enable clock to Timer 3
rccptr->APB1ENR |= RCC_APB1ENR_TIM3EN; rccptr->APB1RSTR |= RCC_APB1RSTR_TIM3RST; //reset timer 3// Configure the pin as timer 3 counter 1 output
GPIOA->AFR[0] |= 0x01000000; //pin PA6 - alternate function 1 (TIM3_CH1) GPIOA->MODER |= 0x00002000; //set PA6 to ''alternate function''// Configure timer 3 channel 1
TIM3->CCMR1 = 0x0068; //PWM mode 1; output; preload enable TIM3->CCER = 0x0001; //CC1 is output to pin TIM3->PSC = 1 - 1; TIM3->ARR = 40000 - 1; TIM3->CCR1 = 300; TIM3->CR1 |= 0x0001; //start the counter The issue is that the output pin (pin 16) does not change - always low. What am I missing?