Skip to main content
Md Mubdiul Hasan
Associate III
October 19, 2016
Question

stm32f0 SPI1 Unidirectional receive-only procedure

  • October 19, 2016
  • 2 replies
  • 484 views
Posted on October 19, 2016 at 09:56

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    2 replies

    slimen
    Visitor II
    October 19, 2016
    Posted on October 19, 2016 at 18:11

    Hello,

    I suggest, as a first step, to run one of the SPI Full Duplex example in STM32CubeF0 firmware with a similar type of your project. Compare the code/functions with your project: STM32Cube_FW_F0_V1.6.0\Projects\STM32F0308-Discovery\Examples\SPI

     

    Regards

    Md Mubdiul Hasan
    Associate III
    October 20, 2016
    Posted on October 20, 2016 at 09:11

    Dear Sir,

    I saw your mentioned code.

    My board is custom one.

    Can you kindly make some comment about send/receive bytes and  conditioning DMA/SPI registerS?