Associate II
September 4, 2014
Question
STM32F0 spi clock problem
- September 4, 2014
- 6 replies
- 1474 views
Posted on September 04, 2014 at 12:29
Hi!
I'm trying to communicate with Atmel AT45DB081D dataflash over SPI. For testing I've send command to read Manufacturer and Device ID (0x9F on MOSI). After I've sent data, SPI clock stops to pulse and, I assume, slave is not able to send any data because clock is not present. This is my first time using SPI on STM32F0. Screenshot is attached below. (SCK-green, MOSI-yellow, CS-blue, MISO-red). Any suggestions how to force SPI clock to continue?/public/STe2ecommunities/mcu/Lists/STM32Discovery/Attachments/11972/scope_0.bmp
Here is the SPI initialization:void SPI1_Config(void)
{
SPI_InitTypeDef SPI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable the SPI periph */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
/* Enable SCK, MOSI, MISO and NSS GPIO clocks */
RCC_AHBPeriphClockCmd(SPI1_SCK_GPIO_CLK | SPI1_MISO_GPIO_CLK | SPI1_MOSI_GPIO_CLK | SPI1_NSS_GPIO_CLK, ENABLE);
GPIO_PinAFConfig(SPI1_SCK_GPIO_PORT, SPI1_SCK_SOURCE, SPI1_SCK_AF);
GPIO_PinAFConfig(SPI1_MOSI_GPIO_PORT, SPI1_MOSI_SOURCE, SPI1_MOSI_AF);
GPIO_PinAFConfig(SPI1_MISO_GPIO_PORT, SPI1_MISO_SOURCE, SPI1_MISO_AF);
GPIO_PinAFConfig(SPI1_NSS_GPIO_PORT, SPI1_NSS_SOURCE, SPI1_NSS_AF);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3;
/* SPI SCK pin configuration */
GPIO_InitStructure.GPIO_Pin = SPI1_SCK_PIN;
GPIO_Init(SPI1_SCK_GPIO_PORT, &GPIO_InitStructure);
/* SPI MOSI pin configuration */
GPIO_InitStructure.GPIO_Pin = SPI1_MOSI_PIN;
GPIO_Init(SPI1_MOSI_GPIO_PORT, &GPIO_InitStructure);
/* SPI MISO pin configuration */
GPIO_InitStructure.GPIO_Pin = SPI1_MISO_PIN;
GPIO_Init(SPI1_MISO_GPIO_PORT, &GPIO_InitStructure);
/* SPI NSS pin configuration */
GPIO_InitStructure.GPIO_Pin = SPI1_NSS_PIN;
GPIO_Init(SPI1_NSS_GPIO_PORT, &GPIO_InitStructure);
/* SPI configuration -------------------------------------------------------*/
SPI_I2S_DeInit(SPI1);
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Hard;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
/* Configure the SPI interrupt priority */
NVIC_InitStructure.NVIC_IRQChannel = SPI1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* Initializes the SPI communication */
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_Init(SPI1, &SPI_InitStructure);
/* Initialize the FIFO threshold */
SPI_RxFIFOThresholdConfig(SPI1, SPI_RxFIFOThreshold_QF);
/* Enable the Rx buffer not empty interrupt */
SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE);
/* Enable the SPI Error interrupt */
SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_ERR, ENABLE);
/* Enable NSS output for master mode */
SPI_SSOutputCmd(SPI1, ENABLE);
SPI_NSSPulseModeCmd(SPI1, ENABLE);
/* Enable the SPI peripheral */
SPI_Cmd(SPI1, ENABLE);
}
Thanks,
Zlatko