Skip to main content
felisleonline
Visitor II
August 2, 2016
Question

STM32F0 reading internal temperature sensor and reference voltage at the same time.

Posted on August 02, 2016 at 21:25

Hi ,

I interested in measuring STM32F0 temperature and reference voltage using internal sensor of it's processor at the same time using UART. so I used channels like this;

ADC_ChannelConfig(ADC1, ADC_Channel_16 , ADC_SampleTime_55_5Cycles);

ADC_TempSensorCmd(ENABLE);

ADC_ChannelConfig(ADC1, ADC_Channel_Vrefint , ADC_SampleTime_55_5Cycles);

ADC_VrefintCmd(ENABLE);

Now I can measured only one values properly..If I applied to read two channel at the same time.I mixed volues eachother. I also looked for multichannel adc titles in the forum but it didn't work properly again. I think should use dma but I'm not good now.Thank you in advance for your help.

Regards.
    This topic has been closed for replies.

    2 replies

    Amel NASRI
    ST Technical Moderator
    August 22, 2016
    Posted on August 22, 2016 at 17:13

    Hi felisleo,

    I suggest you have a look to the 2 following examples available in the

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubef0.html

    package:

    - STM32Cube_FW_F0_V1.6.0\Projects\STM32F072RB-Nucleo\Examples_LL\ADC\ADC_MultiChannelSingleConversion

    - STM32Cube_FW_F0_V1.6.0\Projects\STM32F072RB-Nucleo\Examples\ADC\ADC_Sequencer

    In both examples, the two internal channels (temperature sensor and VrefInt) are converted.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Tesla DeLorean
    Guru
    August 22, 2016
    Posted on August 22, 2016 at 20:41

    If you have two channels DMAing into an array in continuous/circular fashion you shouldn't get them mixed up. So I'm assuming you're trying to poll them.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..