Skip to main content
angeliran
Associate III
September 22, 2015
Question

stm32f0 help with flash, to read and write + hal libraries

Posted on September 22, 2015 at 22:29

Hi all, I wonder if anyone knows how to read and write to the flash stm32f0, using hal libraries ?. What I hold, it is to store some values ​​in real time, and when you restart the device, are present (such as EEPROM of the pics, and I know what are the differences between flash and EEPROM). Basically I read that in order to write, you have to unlock with:

HAL_FLASH_Unlock (void);

Then, you have to delete, either by page, or if all with:

FLASH_EraseInitTypeDef erase_pages;

erase_pages.PageAddress = 0x08000000;

erase_pages.NbPages = 1;

erase_pages.TypeErase = TYPEERASE_PAGES;

uint32_t * Error;

// To write this done BEFORE

HAL_FLASH_Unlock ();

HAL_FLASHEx_Erase (& erase_pages, error);

HAL_FLASH_Lock ();

// WRITE ONLY AFTER AN ERASE PAGE

HAL_FLASH_Unlock ();

  HAL_FLASH_Program (TYPEPROGRAM_HALFWORD, 0x08000000, Data_config [0]);

HAL_FLASH_Lock ();

// READ

Data_config [0] = * ((uint16_t *) 0x08000000); // Read flash memory at address 0x08000000

From here, it stays stuck in:

HAL_FLASHEx_Erase (& erase_pages, error);

I know the flash memory starts at: 0x08000000, and only occupy one page to try to record a value, switch off the device, read, and verify that indeed the recorded data is left.

I guess I'm pounding of the code, for that reason, don´t advance, i tell to you that I do not use bootloader.

Greetings, and if someone could give me a guide, they are grateful enough.
    This topic has been closed for replies.

    12 replies

    Tesla DeLorean
    Guru
    September 22, 2015
    Posted on September 22, 2015 at 22:36

    And where is this code residing? 0x08000000 doesn't sound like a good place to start testing.

    Pick some where that's not sitting on top of your code, and step through it with the debugger, or instrument it with USART output. You shouldn't need to Lock/Unlock between operations. Look for HAL examples under the Cube installation.

    How big is the FLASH in the part you're using? Start at the back end and move downward.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    angeliran
    angeliranAuthor
    Associate III
    September 22, 2015
    Posted on September 23, 2015 at 01:32

    Hi clive1, thx for answering.

    I have tried in page 60, according to RM, the direction: 0x0800F00c, with the same result. I´ve use stmstudio, to check the variables, but, it hang when go to:

    HAL_FLASHEx_Erase(&erase_pages, errores);

    The board is stm32f0 discovery, with stm32f051r8 ic, it has 64 kb of flash.

    Tesla DeLorean
    Guru
    September 23, 2015
    Posted on September 23, 2015 at 02:21

     0x0800FC00 - assuming each block is 0x400

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    angeliran
    angeliranAuthor
    Associate III
    September 24, 2015
    Posted on September 24, 2015 at 18:36

    Yes, 0x0800Fc00, but same result, i've continue check it...

    angeliran
    angeliranAuthor
    Associate III
    September 25, 2015
    Posted on September 25, 2015 at 20:47

    There are some case, that it write it, but when i´ll try to isolate, it don't write... i´ll try to do only that part, not in my main program...

    UPDATE:

    No luck...

    UPDATE2: 

    I tried to upload some pictures, but the server has problems. Basically, I am using the Keil debugger, but does not show me a registry change

    FLASH / AR

    with the instruction:

    WRITE_REG (FLASH-> AR, 0x08007000);

    UPDATE3:

    in desperation, I wrote directly to the memory address register AR with:

    WRITE_REG ((* (uint32_t *) 0x40022014), 0x08007000);

    And again, no luck ...

      WRITE_REG((*(uint32_t *)0x40022014), 0x08007000);

    Tesla DeLorean
    Guru
    September 26, 2015
    Posted on September 26, 2015 at 19:46

    Ok, got some fundamental pointer issues there

    &FLASH->AR /* The address OF the register, not the content */ 0x40022014 /* The ADDRESS, not the content at the address */ You should perhaps pay attention to errors returned by the routines, and ensure the flash status is cleared of errors before you start. The HAL/F0 really aren't things I'm working with, I've posted FLASH code for SPL/F0 It would look something like

    /* Unlock the Flash to enable the flash control register access *************/
    FLASH_Unlock();
    /* Erase the user Flash area */
    /* Clear pending flags (if any) */
    FLASH_ClearFlag(FLASH_FLAG_EOP | FLASH_FLAG_PGERR | FLASH_FLAG_WRPERR);
    if (FLASH_ErasePage(0x08007000)!= FLASH_COMPLETE)
    {
    /* Error occurred while sector erase.
    User can add here some code to deal with this error */
    while (1)
    {
    }
    }
    /* Program the user Flash area word by word */
    Address = 0x08007000;
    while (Address < 0x08007014)
    {
    if (FLASH_ProgramWord(Address, DATA_32) == FLASH_COMPLETE)
    {
    Address = Address + 4;
    }
    else
    {
    /* Error occurred while writing data in Flash memory.
    User can add here some code to deal with this error */
    while (1)
    {
    }
    }
    }
    /* Lock the Flash to disable the flash control register access (recommended
    to protect the FLASH memory against possible unwanted operation) *********/
    FLASH_Lock();

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    angeliran
    angeliranAuthor
    Associate III
    September 27, 2015
    Posted on September 27, 2015 at 02:08

    Thanks for answering clive, the FLASH-> AR register, contains the begin memory address, that we want to erase?

    So, in keil, in debug mode, i saw, the address of FLASH-> AR register, was: 0x40022014, so, i want to put in that address, 0x08007000, that represent, where i want to erase one page, with enabling bit:   SET_BIT(FLASH->CR, FLASH_CR_STRT); or i´m wrong?

    Sorry for your headaches, jeje.

    I´ll check your sugestion, but yes or yes, i need to modify the iROM section?

    I´ll try to adapt to HAL libraries.

    Tesla DeLorean
    Guru
    September 27, 2015
    Posted on September 27, 2015 at 03:22

    I'm not familiar with the MACRO's you're using

    But I'm pretty sure that

    WRITE_REG (FLASH-> AR, 0x08007000);

    Is NOT the equivalent of

    FLASH->AR = 0x08007000;

    Because you're randomly mixing what's a pointer (an address) and what's the value (content at an address).

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    angeliran
    angeliranAuthor
    Associate III
    September 27, 2015
    Posted on September 28, 2015 at 01:50

    Ok Clive, i´ve try your advices, and post results, thx!

    angeliran
    angeliranAuthor
    Associate III
    September 28, 2015
    Posted on September 28, 2015 at 21:08

    Ok clive, thx for your help!!!, only work with this 7 steps, with f0/ha1: 

    HAL_FLASH_Unlock();

    FLASH->CR |= FLASH_CR_PER; /* (1) */

    FLASH->AR = 0x0800e400; /* (2) */

    FLASH->CR |= FLASH_CR_STRT; /* (3) */

    while ((FLASH->SR & FLASH_SR_BSY) != 0) /* (4) */

    {/* For robust implementation, add here time-out management */}

    if ((FLASH->SR & FLASH_SR_EOP) != 0) /* (5) */

    {FLASH->SR |= FLASH_SR_EOP; /* (6)*/}

    else

    {/* Manage the error cases */}

    FLASH->CR &= ~FLASH_CR_PER; /* (7) */

    HAL_FLASH_Program(TYPEPROGRAM_HALFWORD, 0x0800e400, 0x5678);

    HAL_FLASH_Lock();

    uint16_t dato;

      /* Infinite loop */

      /* USER CODE BEGIN WHILE */

      while (1){ 

    dato=*((uint16_t *) 0x0800e400);

    if (dato==0x5678){

    HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_9);}

    HAL_Delay(500);}

      /* USER CODE END 3 */

    }

    I need to do more tests, for example, check if the data continue there, at the moment of excitement, I wanted to share this achievement, hehe...

    UPDATE:

    It work! doing power cycle, the data is there. The last doubts Clive, did you know why need to do the hole between iROM1 and iROM2? why not only cut at the end with one iROM?