Skip to main content
guitarman87
Visitor II
February 17, 2016
Question

STM32F0 EXTI Port unusable

  • February 17, 2016
  • 1 reply
  • 775 views
Posted on February 17, 2016 at 12:50

Hello,

I noticed a problem with the STM32F030F4P6 Microcontroller.

When I configure EXTI Line 0 and 1 with GPIOF =>

PF0,PF1 are my EXTI for two Light Fork Barrier Modules.

then all of the sudden my PB1 Pin can't be toggled(and yes I initialized it).

Is this a known issue that EXTI Line 1 Config disables other Port Pins with 1?

(For Example PA1,PB1,PC1 ect.)

I can upload code example if needed.

Thanks.

#stm32f0-problem-unusable-pin
This topic has been closed for replies.

1 reply

waclawek.jan
Super User
February 17, 2016
Posted on February 17, 2016 at 13:14

Disable interrupts.

Still can't toggle PB1?

JW