Question
STM32F0 deep sleep with TIM1 as time-base source
Posted on April 09, 2018 at 10:49
Hi,
I having a problem to get in sleep mode when using TIM1 as time-base source instead sysTick.
When using sysTick I'm able to enter sleep mode with no problem.
I wish to use TIM1 as time-base source to be able to use freeRTOS in the future.
What is wrong with this simple example?
while (1)
{ blinkLED(); if(btnPressed) { HAL_SuspendTick(); HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI); HAL_ResumeTick(); } }void blinkLED()
{ HAL_GPIO_WritePin(LED3_GPIO_Port, LED3_Pin, 0); HAL_Delay(100); HAL_GPIO_WritePin(LED3_GPIO_Port, LED3_Pin, 1); HAL_Delay(100);}void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin){ if (GPIO_Pin == BTN_Pin) { if(btnPressed) btnPressed = 0; else btnPressed = 1; }}