STM32F0 ADC->DMA touble
I have looked over the following code many times. Not sure what the problem is. Any incite? The raw_dma_adc[] array has no values in it during debug.
The code is for a STM32F051K6U6. End goal is to have 5 channels running. GPIO clock for port A has been enabled.///////////////////////ADC
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2| GPIO_Pin_3 | GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1 , ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);ADC_DeInit(ADC1);
DMA_DeInit(DMA1);ADC_InitTypeDef Impac_ADC;
Impac_ADC.ADC_Resolution = ADC_Resolution_12b; Impac_ADC.ADC_ContinuousConvMode = ENABLE; Impac_ADC.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; Impac_ADC.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_TRGO; //not used Impac_ADC.ADC_DataAlign = ADC_DataAlign_Right; Impac_ADC.ADC_ScanDirection = ADC_ScanDirection_Backward; ADC_Init(ADC1, &Impac_ADC);ADC_ChannelConfig(ADC1, ADC_Channel_0, ADC_SampleTime_239_5Cycles);
ADC_ChannelConfig(ADC1, ADC_Channel_1, ADC_SampleTime_239_5Cycles);
//Calibrate ADC. This must be done before enabling the ADC. The function has a delay built in to allow for wait for calibration.
ADC_GetCalibrationFactor(ADC1);ADC_DMARequestModeConfig(ADC1, ADC_DMAMode_Circular);
DMA_InitTypeDef Impac_DMA;
Impac_DMA.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR; Impac_DMA.DMA_MemoryBaseAddr = (uint32_t)&raw_dma_adc[0]; Impac_DMA.DMA_DIR = DMA_DIR_PeripheralSRC;//? //DMA_DIR_PeripheralSRC; Impac_DMA.DMA_BufferSize = 2; Impac_DMA.DMA_PeripheralInc = DMA_PeripheralInc_Enable; //Keep incrimenting pointer to ADC buffer as tranfering. Impac_DMA.DMA_MemoryInc = DMA_MemoryInc_Enable; //Keep incrimenting pointer to DMA mem Impac_DMA.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; Impac_DMA.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; Impac_DMA.DMA_Mode = DMA_Mode_Circular; Impac_DMA.DMA_Priority = DMA_Priority_High; Impac_DMA.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1, &Impac_DMA); ADC_DMACmd(ADC1, ENABLE); ADC_Cmd(ADC1, ENABLE); DMA_Cmd(DMA1_Channel1, ENABLE);ADC_StartOfConversion(ADC1);