Skip to main content
danielblesener9
Associate III
March 26, 2014
Question

STM32F0 ADC->DMA touble

  • March 26, 2014
  • 15 replies
  • 2249 views
Posted on March 26, 2014 at 16:54

I have looked over the following code many times. Not sure what the problem is. Any incite? The raw_dma_adc[] array has no values in it during debug.

The code is for a STM32F051K6U6. End goal is to have 5 channels running. GPIO clock for port A has been enabled.

    ///////////////////////ADC

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2| GPIO_Pin_3 | GPIO_Pin_4;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1 , ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

    ADC_DeInit(ADC1);

    DMA_DeInit(DMA1);

    ADC_InitTypeDef Impac_ADC;

    Impac_ADC.ADC_Resolution = ADC_Resolution_12b;

    Impac_ADC.ADC_ContinuousConvMode = ENABLE;

    Impac_ADC.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

    Impac_ADC.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_TRGO; //not used

    Impac_ADC.ADC_DataAlign = ADC_DataAlign_Right;

    Impac_ADC.ADC_ScanDirection = ADC_ScanDirection_Backward;

    ADC_Init(ADC1, &Impac_ADC);

    ADC_ChannelConfig(ADC1, ADC_Channel_0, ADC_SampleTime_239_5Cycles);

    ADC_ChannelConfig(ADC1, ADC_Channel_1, ADC_SampleTime_239_5Cycles);

    //Calibrate ADC. This must be done before enabling the ADC. The function has a delay built in to allow for wait for calibration.

    ADC_GetCalibrationFactor(ADC1);

    ADC_DMARequestModeConfig(ADC1, ADC_DMAMode_Circular);

    DMA_InitTypeDef Impac_DMA;

    Impac_DMA.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;

    Impac_DMA.DMA_MemoryBaseAddr = (uint32_t)&raw_dma_adc[0];

    Impac_DMA.DMA_DIR = DMA_DIR_PeripheralSRC;//? //DMA_DIR_PeripheralSRC;

    Impac_DMA.DMA_BufferSize = 2;

    Impac_DMA.DMA_PeripheralInc = DMA_PeripheralInc_Enable;         //Keep incrimenting pointer to ADC buffer as tranfering.

    Impac_DMA.DMA_MemoryInc = DMA_MemoryInc_Enable;                 //Keep incrimenting pointer to DMA mem

    Impac_DMA.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;

    Impac_DMA.DMA_MemoryDataSize = DMA_MemoryDataSize_Word;

    Impac_DMA.DMA_Mode = DMA_Mode_Circular;

    Impac_DMA.DMA_Priority = DMA_Priority_High;

    Impac_DMA.DMA_M2M = DMA_M2M_Disable;

    DMA_Init(DMA1, &Impac_DMA);

   

    ADC_DMACmd(ADC1, ENABLE);

   

    ADC_Cmd(ADC1, ENABLE);

   

    DMA_Cmd(DMA1_Channel1, ENABLE);

    ADC_StartOfConversion(ADC1);

    This topic has been closed for replies.

    15 replies

    stm322399
    Senior
    March 26, 2014
    Posted on March 26, 2014 at 17:06

    Let's begin with changing

        Impac_DMA.DMA_PeripheralInc = DMA_PeripheralInc_Enable;         //Keep incrimenting pointer to ADC buffer as tranfering.

    with non-incrementing configuration, so the DMA always read the DR register.

    Tesla DeLorean
    Guru
    March 26, 2014
    Posted on March 26, 2014 at 17:35

    That, and probably not 32-bit words either.

    // STM32 ADC 4 Channel DMA/TIM STM32F0-Discovery sourcer32@gmail.com
    #include ''stm32f0xx.h''
    //**************************************************************************************
    #define SAMPLES 200
    __IO uint16_t RegularConvData[SAMPLES]; // 100 Samples to half, 25 x 4, Calls IRQ at 40 Hz
    void ADC_TIM_DMA_Config(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_OCInitTypeDef TIM_OCInitStructure;
    ADC_InitTypeDef ADC_InitStructure;
    DMA_InitTypeDef DMA_InitStructure;
    /* ADC1 DeInit */
    ADC_DeInit(ADC1);
    /* ADC1 Periph clock enable */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_TIM1, ENABLE);
    /* DMA1 clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
    /* TIM2 Configuration */
    TIM_DeInit(TIM1);
    /* Time base configuration */
    TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
    TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // 1 MHz, from 48 MHz
    TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // 1 KHz
    TIM_TimeBaseStructure.TIM_ClockDivision = 0x0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
    /* Output Compare PWM Mode configuration */
    TIM_OCStructInit(&TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; /* low edge by default */
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_Pulse = 0x01;
    TIM_OC4Init(TIM1, &TIM_OCInitStructure);
    /* TIM1 enable counter */
    TIM_Cmd(TIM1, ENABLE);
    /* Main Output Enable */
    TIM_CtrlPWMOutputs(TIM1, ENABLE);
    /* DMA1 Channel1 Config */
    DMA_DeInit(DMA1_Channel1);
    DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
    DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&RegularConvData[0];
    DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
    DMA_InitStructure.DMA_BufferSize = SAMPLES;
    DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
    DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
    DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
    DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
    DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
    DMA_InitStructure.DMA_Priority = DMA_Priority_High;
    DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
    DMA_Init(DMA1_Channel1, &DMA_InitStructure);
    /* DMA1 Channel1 enable */
    DMA_Cmd(DMA1_Channel1, ENABLE);
    /* ADC DMA request in circular mode */
    ADC_DMARequestModeConfig(ADC1, ADC_DMAMode_Circular);
    /* Enable DMA1 Channel1 Half Transfer and Transfer Complete interrupt */
    DMA_ITConfig(DMA1_Channel1, DMA_IT_HT, ENABLE);
    DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE);
    /* Enable ADC_DMA */
    ADC_DMACmd(ADC1, ENABLE);
    /* Initialize ADC structure */
    ADC_StructInit(&ADC_InitStructure);
    /* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits */
    ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
    ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising;
    ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC4;
    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
    ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;
    ADC_Init(ADC1, &ADC_InitStructure);
    /* Convert the ADC_Channnel_0 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_0 , ADC_SampleTime_7_5Cycles);
    /* Convert the ADC_Channnel_1 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_1 , ADC_SampleTime_7_5Cycles);
    /* Convert the ADC_Channnel_2 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_2 , ADC_SampleTime_7_5Cycles);
    /* Convert the ADC_Channnel_3 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_3 , ADC_SampleTime_7_5Cycles);
    /* ADC Calibration */
    ADC_GetCalibrationFactor(ADC1);
    /* Enable ADC1 */
    ADC_Cmd(ADC1, ENABLE);
    /* Wait the ADCEN flag */
    while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN));
    /* ADC1 regular Software Start Conv */
    ADC_StartOfConversion(ADC1);
    }
    //**************************************************************************************
    void DMA1_Channel1_IRQHandler(void) // Called at 40 Hz, LED Toggles at 20 Hz
    {
    /* Test on DMA1 Channel1 Transfer Complete interrupt */
    if (DMA_GetITStatus(DMA1_IT_HT1))
    {
    /* Clear DMA1 Channel1 Half Transfer interrupt pending bits */
    DMA_ClearITPendingBit(DMA1_IT_HT1);
    GPIOC->BSRR = 0x300; /* Set PC8 and PC9 */
    }
    /* Test on DMA1 Channel1 Transfer Complete interrupt */
    if (DMA_GetITStatus(DMA1_IT_TC1))
    {
    /* Clear DMA1 Channel1 Transfer Complete interrupt pending bits */
    DMA_ClearITPendingBit(DMA1_IT_TC1);
    GPIOC->BRR = 0x300;/* Reset PC8 and PC9 */
    }
    }
    //**************************************************************************************
    void NVIC_Config(void)
    {
    NVIC_InitTypeDef NVIC_InitStructure;
    /* Enable and set DMA1_Channel1 Interrupt */
    NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn;
    NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00;
    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
    NVIC_Init(&NVIC_InitStructure);
    }
    //**************************************************************************************
    void GPIO_Config(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /* GPIOC Periph clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
    /* Configure PC8 and PC9 in output pushpull mode */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    /* GPIOA Periph clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
    /* Configure ADC Channels as analog input - might conflict */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    }
    //**************************************************************************************
    int main(void)
    {
    NVIC_Config();
    GPIO_Config();
    ADC_TIM_DMA_Config();
    while(1); /* Infinite loop */
    }
    //**************************************************************************************
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* Infinite loop */
    while (1)
    {
    }
    }
    #endif
    //**************************************************************************************

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    March 26, 2014
    Posted on March 26, 2014 at 17:43

    // STM32 ADC 5 Channel DMA/TIM STM32F0-Discovery sourcer32@gmail.com
    #include ''stm32f0xx.h''
    //**************************************************************************************
    #define SAMPLES 2500
    __IO uint16_t RegularConvData[SAMPLES]; // 1250 Samples to half, 250 x 5, Calls IRQ at 4 Hz (1KHZ/250)
    void ADC_TIM_DMA_Config(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_OCInitTypeDef TIM_OCInitStructure;
    ADC_InitTypeDef ADC_InitStructure;
    DMA_InitTypeDef DMA_InitStructure;
    /* ADC1 DeInit */
    ADC_DeInit(ADC1);
    /* ADC1 Periph clock enable */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_TIM1, ENABLE);
    /* DMA1 clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
    /* TIM2 Configuration */
    TIM_DeInit(TIM1);
    /* Time base configuration */
    TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
    TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // 1 MHz, from 48 MHz
    TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // 1 KHz
    TIM_TimeBaseStructure.TIM_ClockDivision = 0x0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
    /* Output Compare PWM Mode configuration */
    TIM_OCStructInit(&TIM_OCInitStructure);
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; /* low edge by default */
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_Pulse = 0x01;
    TIM_OC4Init(TIM1, &TIM_OCInitStructure);
    /* TIM1 enable counter */
    TIM_Cmd(TIM1, ENABLE);
    /* Main Output Enable */
    TIM_CtrlPWMOutputs(TIM1, ENABLE);
    /* DMA1 Channel1 Config */
    DMA_DeInit(DMA1_Channel1);
    DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
    DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&RegularConvData[0];
    DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
    DMA_InitStructure.DMA_BufferSize = SAMPLES;
    DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
    DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
    DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
    DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
    DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
    DMA_InitStructure.DMA_Priority = DMA_Priority_High;
    DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
    DMA_Init(DMA1_Channel1, &DMA_InitStructure);
    /* DMA1 Channel1 enable */
    DMA_Cmd(DMA1_Channel1, ENABLE);
    /* ADC DMA request in circular mode */
    ADC_DMARequestModeConfig(ADC1, ADC_DMAMode_Circular);
    /* Enable DMA1 Channel1 Half Transfer and Transfer Complete interrupt */
    DMA_ITConfig(DMA1_Channel1, DMA_IT_HT, ENABLE);
    DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE);
    /* Enable ADC_DMA */
    ADC_DMACmd(ADC1, ENABLE);
    /* Initialize ADC structure */
    ADC_StructInit(&ADC_InitStructure);
    /* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits */
    ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
    ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising;
    ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC4;
    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
    ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;
    ADC_Init(ADC1, &ADC_InitStructure);
    /* Convert the ADC_Channnel_0 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_0 , ADC_SampleTime_7_5Cycles);
    /* Convert the ADC_Channnel_1 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_1 , ADC_SampleTime_7_5Cycles);
    /* Convert the ADC_Channnel_2 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_2 , ADC_SampleTime_7_5Cycles);
    /* Convert the ADC_Channnel_3 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_3 , ADC_SampleTime_7_5Cycles);
    /* Convert the ADC_Channnel_4 with 7.5 Cycles as sampling time */
    ADC_ChannelConfig(ADC1, ADC_Channel_4 , ADC_SampleTime_7_5Cycles);
    /* ADC Calibration */
    ADC_GetCalibrationFactor(ADC1);
    /* Enable ADC1 */
    ADC_Cmd(ADC1, ENABLE);
    /* Wait the ADCEN flag */
    while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN));
    /* ADC1 regular Software Start Conv */
    ADC_StartOfConversion(ADC1);
    }
    //**************************************************************************************
    void DMA1_Channel1_IRQHandler(void) // Called at 4 Hz, LED Toggles at 2 Hz
    {
    /* Test on DMA1 Channel1 Transfer Complete interrupt */
    if (DMA_GetITStatus(DMA1_IT_HT1))
    {
    /* Clear DMA1 Channel1 Half Transfer interrupt pending bits */
    DMA_ClearITPendingBit(DMA1_IT_HT1);
    GPIOC->BSRR = 0x100; /* Set PC8 */
    GPIOC->BRR = 0x200;/* Reset PC9 */
    }
    /* Test on DMA1 Channel1 Transfer Complete interrupt */
    if (DMA_GetITStatus(DMA1_IT_TC1))
    {
    /* Clear DMA1 Channel1 Transfer Complete interrupt pending bits */
    DMA_ClearITPendingBit(DMA1_IT_TC1);
    GPIOC->BSRR = 0x200; /* Set PC9 */
    GPIOC->BRR = 0x100;/* Reset PC8 */
    }
    }
    //**************************************************************************************
    void NVIC_Config(void)
    {
    NVIC_InitTypeDef NVIC_InitStructure;
    /* Enable and set DMA1_Channel1 Interrupt */
    NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn;
    NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00;
    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
    NVIC_Init(&NVIC_InitStructure);
    }
    //**************************************************************************************
    void GPIO_Config(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    /* GPIOC Periph clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
    /* Configure PC8 and PC9 in output pushpull mode */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    /* GPIOA Periph clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
    /* Configure ADC Channels as analog input - might conflict */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    }
    //**************************************************************************************
    int main(void)
    {
    NVIC_Config();
    GPIO_Config();
    ADC_TIM_DMA_Config();
    while(1); /* Infinite loop */
    }
    //**************************************************************************************
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* Infinite loop */
    while (1)
    {
    }
    }
    #endif
    //**************************************************************************************

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    danielblesener9
    Associate III
    March 26, 2014
    Posted on March 26, 2014 at 19:00

    Thank you for the replies. I have tried making the requested changes, excluding adding interrupt to DMA. I will try this though.

    I changed the word size to half, Impac_DMA.DMA_PeripheralInc = DMA_PeripheralInc_Disable, and changed the counting to upward. I should note that I am doing nothing in my main loop. I am just watching the array where the data should be transferred to expecting to see something when the program runs. I made all of these individually hoping one of them alone was an issue.

    I am surprised to not see any DMA transfer. This worked great for me on the STM32F1. Any other ideas?

    Tesla DeLorean
    Guru
    March 26, 2014
    Posted on March 26, 2014 at 20:19

    DMA_DeInit(DMA1, &Impac_DMA);   DMA_Init(DMA1, &Impac_DMA);

    DMA1_Channel1 ??
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    danielblesener9
    Associate III
    March 28, 2014
    Posted on March 28, 2014 at 15:02

    Clive - still no luck.

    I copied in your example code and it works. I removed the interrupt - still works.

    When I attempt to remove timer 1, or even just

      /* Output Compare PWM Mode configuration */

      TIM_OCStructInit(&TIM_OCInitStructure);

      TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; /* low edge by default */

      TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

      TIM_OCInitStructure.TIM_Pulse = 0x01;

      TIM_OC4Init(TIM1, &TIM_OCInitStructure);

      /* Main Output Enable */

      TIM_CtrlPWMOutputs(TIM1, ENABLE);

    the DMA does not work. I do not understand why the DMA needs the pwm output compare or TIM1 for successful operation? Can you explain this?

    Tesla DeLorean
    Guru
    March 28, 2014
    Posted on March 28, 2014 at 15:18

    I am pacing the sampling at a designated frequency, rather than attempting to free run the ADC.

    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising;
    ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC4;

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    danielblesener9
    Associate III
    March 31, 2014
    Posted on March 31, 2014 at 16:55

    That makes sense. Thanks again for the help Clive. All of the engineers here at PEM want to thank you for your continued support. You have solved a problem with a stm MCU for all of us at some point or another.

    entwicklung
    Associate III
    June 6, 2014
    Posted on June 06, 2014 at 09:06

    The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6fU&d=%2Fa%2F0X0000000bsn%2FIH9iDjZRNreIttbeL.lapotIZqP.lPS.jkw1tuDteyc&asPdf=false
    Tesla DeLorean
    Guru
    June 6, 2014
    Posted on June 06, 2014 at 14:09

    For just four values in to memory, I probably wouldn't use the TC/HT interrupts in this fashion.

    The USART output sends 8-bit binary bytes, not sure how helpful that is as the numbers are 12-bit, and an ASCII decimal output would be easier to view on a terminal.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..